A question about UART interrupt
In order to configure UART interrupt receive, I put HAL_UART_Receive_IT function in HAL_UART_RxCpltCallback.
but it doesnt work. below is my callback code.
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{ uint8_t i; if (huart->Instance == USART2) //current UART { if (Rx_indx==0) {for (i=0;i<RXBUFFERBYTE;i++) aRxBuffer[i]=0;} //clear Rx_Buffer before receiving new data if (Rx_data[0]!=10) //if received data different from ascii 10 { aRxBuffer[Rx_indx++]=Rx_data[0]; //add data to Rx_Buffer } else //if received data = 10 { Rx_indx=0; USART2_RX_STANBY=1;//transfer complete, data is ready to read } if(HAL_UART_Receive_IT(&huart2,Rx_data, 1) != HAL_OK)//activate UART receive interrupt every time { Error_Handler(); } } }The main program has HAL_UART_Receive_IT in beginning part. so i put some character of ASCII and my program reach if(HAL_UART_Receive_IT(&huart2,Rx_data, 1) != HAL_OK) . I checked that HAL_UART_Receive_IT returned HAL_OK then it means preparation of UART receive interrupt.
but the program doenst take interrupt when I send ASCII to MCU.
I have no clue.. anyone who have had same experience??
help me please.
Thank you.