APMemory APS12808 OSPI memory connection to STM32H723ZGT6
- August 27, 2025
- 7 replies
- 1610 views
Hello,
I am writing to seek advice on connecting an APMemory APS12808 OSPI memory to the STM32H723ZGT6 microcontroller.
Initially, I attempted to adapt the code from this thread ( https://community.st.com/t5/stm32-mcus-products/stm32h7-octospi-mode-hyperbus-hyperram-access-and-delay-block/td-p/143237/page/2 ) from
Subsequently, I tried to enable the Memory Mapped mode based on Application Note AN5050. This is where significant problems began I cannot get this mode to activate. The relevant code is in the attached file `main_2.c`.
My specific questions are:
1. Is there a known working example for enabling the Memory Mapped mode for this type of memory?
2. Why does AN5050 not cover the MR (Mode Register) configuration and memory initialization sequence?
3. Is there any functional difference in which OCTOSPI interface (OCTOSPI1 or OCTOSPI2) is used to connect the memory?
4. Is it acceptable to leave the memory's RESET pin unconnected (floating) if it is not being used?
5. Can I use pins with different Alternate Function (AF) numbers within the same OCTOSPI connection (e.g., for data lines), or must they all belong to the same predefined AF group?
6. There is a dedicated driver available here: ( https://github.com/STMicroelectronics/stm32-aps6408 ). How current and reliable is this driver? Are there any usage examples available?
7. In this thread ( https://community.st.com/t5/stm32-mcus-products/unable-to-read-reset-values-of-the-stm32h730vb-octospim/td-p/212094 ), I read about the OCTOSPIM clock being disabled by default. Is this issue still relevant for the STM32H7 series, and are any specific actions required to ensure proper memory operation?
8. On one of my PCB revisions, the memory's B1 pin is accidentally tied to ground. Is this configuration acceptable, or will it prevent the memory from functioning correctly?
Thank you for your assistance.
Best regards, Max