Skip to main content
Visitor II
December 11, 2025
Question

BiSS-C Encoder feedback on EVSPIN32G4

  • December 11, 2025
  • 1 reply
  • 546 views

Hello, 

as in this post i'm linking

Is there a way to use absolute encoders/resolvers ... - STMicroelectronics Community

i need to use a Biss-c absoulte encoder for a servo drive application using BLDC motors with STSPIN32G4, we are testing using EVSPIN32G4.

In the workbench i did not find the configuration for directly feedback through absolute Biss-C encoder. Am i missing something?

Other way to do this could be go through SPI peripheral to read absolute Biss-C encoders, but as asked in the post linked, how could i use SPI data to be used from BLDC controller? 

 

Thanks to everyone helping. 

Jackex

1 reply

GMA
Technical Moderator
December 17, 2025

Hello @Jackex-hw,

Absolute Biss-C encoder interface is not supported by MCSDK.
Refer to previous posts as:
Solved: STM32H7 NUCLEO-H723ZG SPI Master RXONLY mode - how... - STMicroelectronics Community
or
BiSS-C Implementation - STMicroelectronics Community

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA