Skip to main content
Associate
June 26, 2025
Question

Clarification on IWDG Reset Behavior: UM3150 vs RM0481 (STM32H5 Series)

  • June 26, 2025
  • 3 replies
  • 584 views

I came across a discrepancy between two ST documents regarding the behavior of an IWDG reset on STM32H5 devices, and I’d like clarification on what exactly is reset when an IWDG event occurs.

  • Document 1: UM3150 Rev 2 – STM32H5 Safety Manual, Table 9 (CPU_SM_6)
    States that the IWDG reset may result in an "incomplete" local safe state — it only resets the CPU and does not guarantee that application software can bring the system to a final safe state. This implies that I/O and peripherals may not be reset

UM3150.png

  • Document 2: RM0481 Rev 2 – STM32H562/63xx Reference Manual, Section 11.3.2
    States that an IWDG event results in a system reset, and all registers (except RCC_RSR and Backup domain) are returned to their reset values, which implies that peripherals and I/O should also reset.RM0481.png

Can ST clarify this apparent contradiction? Does the IWDG event reset only the CPU (as per UM3150), or the entire system including I/Os and peripherals (as per RM0481)?

 

3 replies

KDJEM.1
Technical Moderator
June 27, 2025

Hello @shivashankarr ;

 

Thank you for bringing this issue to our attention.

I will check this internally and I will get back to you as soon as possible.

Internal ticket number: 213037 (This is an internal tracking number and is not accessible or usable by customers)

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
KDJEM.1
Technical Moderator
June 30, 2025

Hello @shivashankarr;

It mentioned in the Reference Manual the normal behavior, which can be common in several products, not just the STM32H5 family. For further details, the user manual describes the behavior specific to the product. 

The IWDG intervention is able to achieve a potentially “incomplete” local safe state because it can only guarantee that CPU is reset. No guarantee that Application software can be still executed to generate combinations of output signals that might be needed by the external system to achieve the final safe state. If this limitation turn out in a blocking point, End user must adopt CPU_SM_5.  Which may indicate that, in some use cases, it can perform a complete system reset. It depends on the use case of the end user as mentioned in the UM3150.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
July 2, 2025

The concern is UM3150, it states: it can only guarantee that the CPU is reset. No guarantee that the application software can still be executed.”
In safety-critical systems, this raises a concern — we must ensure a complete reset (including internal peripherals and application domain), not just a CPU core reset.

1. I believe the normal expected IWDG behavior is to complete reset (including internal peripherals and application domain). if the IWDG is configured to trigger a complete reset, is there a chance does it in can only reset the CPU on STM32H5-series?

2. On STM32H5-series, under what conditions does the IWDG trigger only a CPU reset (core-only)?

3. If so, what mechanisms or configuration options are available to guarantee that the IWDG triggers a complete reset (i.e., resets both CPU and application domain), as required for safety-critical applications?

 

Thank you.

Shiva

Andrew Neil
Super User
July 2, 2025

@shivashankarr wrote:

The concern is UM3150, it states: it can only guarantee that the CPU is reset. No guarantee that the application software can still be executed.”


But that appears in section 3.6.1, titled "Arm® Cortex®-M33 CPU" - so that section is focussed purely on the CPU.

Other sections address other parts of the chip:

AndrewNeil_0-1751443191913.png

 

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
June 30, 2025

@shivashankarr wrote:
  • Document 2: RM0481 Rev 2 – STM32H562/63xx Reference Manual, Section 11.3.2
    States that an IWDG event results in a system reset, and all registers (except RCC_RSR and Backup domain) are returned to their reset values


In that context, "system" just refers to the STM32 chip.

 


@shivashankarr wrote:
  • which implies that peripherals and I/O should also reset.


"Reset" as in "returned to their power-on defaults".

But, again, that only applies to the internals of the STM32 chip itself - it won't (necessarily) affect anything external to the chip. Your code would need to manage that.

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Tesla DeLorean
Guru
July 2, 2025

Watch things like I2C and QSPI devices lacking an async reset in common with the MCU. These can be left in indeterminate states

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..