Skip to main content
Senior
June 30, 2025
Question

Configuring H7 shared memory as non-caching in MPU causes random hangs

  • June 30, 2025
  • 1 reply
  • 457 views

I've got a program running on a dual-core STM32 (the STM32H747IGT6 if you're curious) and right now it's doing a pile of SCB_CleanDCache_by_Addr() and SCB_InvalidateDCache_by_Addr() to keep shared memory in sync between the CM4 and CM7. I was thinking it would be easier if I just set the shared area to non-cacheable, but when I configure the MPU the system will work for a few seconds and then hang.

The shared memory area is called 'buffer_control' and I padded it to 512 bytes. My MPU configuration looks like this:

SCB_EnableDCache();
SCB_EnableICache();

/* Disable the MPU */
__DMB(); /* Make sure outstanding transfers are done */
SCB->SHCSR &= ~SCB_SHCSR_MEMFAULTENA_Msk; /* Disable fault exceptions */
MPU->CTRL = 0; /* Disable the MPU and clear the control register*/

/* Configure the MPU attributes as WB-WA for SRAM */
MPU->RNR = MPU_REGION_NUMBER0;
MPU->RBAR = (uint32_t)&buffer_control;
MPU->RASR = ((uint32_t)MPU_INSTRUCTION_ACCESS_DISABLE << MPU_RASR_XN_Pos) |
 ((uint32_t)MPU_REGION_FULL_ACCESS << MPU_RASR_AP_Pos) |
 ((uint32_t)MPU_TEX_LEVEL0 << MPU_RASR_TEX_Pos) |
 ((uint32_t)MPU_ACCESS_SHAREABLE << MPU_RASR_S_Pos) |
 ((uint32_t)MPU_ACCESS_NOT_CACHEABLE << MPU_RASR_C_Pos) |
 // ((uint32_t)MPU_ACCESS_NOT_BUFFERABLE << MPU_RASR_B_Pos) |
 // ((uint32_t)MPU_InitStruct.SubRegionDisable << MPU_RASR_SRD_Pos) |
 ((uint32_t)MPU_REGION_SIZE_512B << MPU_RASR_SIZE_Pos) |
 ((uint32_t)MPU_REGION_ENABLE << MPU_RASR_ENABLE_Pos);

/* Enable the MPU */
MPU->CTRL = MPU_PRIVILEGED_DEFAULT | MPU_CTRL_ENABLE_Msk; /* Enable the MPU */
SCB->SHCSR |= SCB_SHCSR_MEMFAULTENA_Msk; /* Enable fault exceptions */
__DSB(); /* Ensure MPU setting take effects */
__ISB();

What am I doing wrong? 

p.s. buffer_control is located at the start of SRAM2 with the address 0x30020000

1 reply

cbcooperAuthor
Senior
June 30, 2025

Note that the only change from "working fine" to "hanging randomly" is the code shown above for configuring the MPU.

mƎALLEm
Technical Moderator
June 30, 2025

Hello,

From the code you posted you are configuring the MPU after enabling the cache which is not recommended. You need to configure the MPU before enabling the cache.

 

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
cbcooperAuthor
Senior
June 30, 2025

Moving 

SCB_EnableDCache();
SCB_EnableICache();

after the other code didn't help any.