Contact DRAM operation using STM32H723ZGT6 OSPI1
Hello
We are working on a new project with STM32H723ZGT6.
I want to control S70KL1283DPBHI020 DRAM with HYPERBUS communication using OSPI1.
If you access 0X900000 memory to write and read data during the current operation, the data will not be read accurately.
It seems necessary to check if there is a problem in the circuit diagram.


I'm using PC2_C pin and PC3_C pin for IO5,6, is it not a problem?
Is it not a problem to use the RESET PIN as a GPIO OUT PIN to give a HIGH signal
I gave the data a value of 0xff up to 100 bytes, but there is another value in the 4th address.
I would like to ask you to check the problem.
Thank you.