Skip to main content
Associate III
December 25, 2024
Question

Couldn't debug via ST-Link

  • December 25, 2024
  • 2 replies
  • 1075 views

Hello,

Just before I tried to debug STM32L052 via ST-Link but following error occurred.

The error message is as following.

It's strange that I could debug and run with same project yesterday and nothing is changed as for project.

What is the problem and how to solve it?

Thanks,

STMicroelectronics ST-LINK GDB server. Version 7.9.0
Copyright (c) 2024, STMicroelectronics. All rights reserved.

Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled

Target unknown error 19

Error in initializing ST-LINK device.
Reason: Unknown. Please check power and cabling to target.

 

2 replies

Technical Moderator
December 25, 2024

Hello @curiae ,

Are you using your own customized board or ST board?

What happens if you connect in STM32CubeProgrammer ? Try to connect through STM32CubeProgrammer and set the connection mode to "Under Reset" and perform a "Full Chip Erase" to clear the flash memory.

Check the debug pins are free, reserved for Debug: How to solve debugger connection issues - STMicroelectronics Community.

If the issue is not resolved, check (through your STM32 schematic and Datasheet) the basic pins and the power supply schemes that are within their specified voltage ranges : VDD, VDDA supply, VCAP pins...

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"
Visitor II
October 21, 2025

Good morning.

I have another problem, that was detected in my ST_link. I used St-Linkv2,  withSTM32 microcontroller and STM Cube IDE program. When I debugged or runned, it says this:

STMicroelectronics ST-LINK GDB server. Version 7.11.0

Copyright (c) 2025, STMicroelectronics. All rights reserved.

 

Starting server with the following options:

Persistent Mode : Disabled

Logging Level : 1

Listen Port Number : 61234

Status Refresh Delay : 15s

Verbose Mode : Disabled

SWD Debug : Enabled

InitWhile : Enabled

 

Target no device found

 

Error in initializing ST-LINK device.

Reason: No device found on target.