CS Glitch with 9-Bit SPI on STM32
Hi everyone,
I’m experiencing unexpected behavior while testing 9-bit SPI on an STM32, observed with a logic analyzer. The issue only occurs when the MOSI line is physically connected to the slave.
Observations:
:keycap_1: MOSI not connected
CS and SCLK are correct
MOSI stays high
SPI decoder shows 0x1FF
Expected behavior for a floating MOSI line
:keycap_2: MOSI connected to the slave
MOSI data becomes correct
But a very brief rising edge (glitch) appears on CS during data transmission
CS immediately returns active → causes unintended slave deselection
Result: data loss during the SPI frame
Additional info:
STM32 model: stm32u5g9j-dk2
SPI mode: 9-bit, master
SCLK frequency: 10 MHz
Is this a known issue with 9-bit SPI on STM32?
Should I add a pull-up/pull-down on CS or MOSI?
Any other suggestions to avoid this glitch?
Attached are screenshots showing the behavior.
Thanks in advance for your help!
MOSI connected
MOSI not connected