Skip to main content
Associate
February 26, 2026
Question

CubeMX not generating PLL2 code for USB using STM32H5

  • February 26, 2026
  • 3 replies
  • 176 views

Hi, 
I am using STM32CubeMX 6.16.1 with a STM32H503RB and I have exactly the same problem : 

clock.png

RCC is configured with LL library (not HAL), here is the SystemClock_Config() function generated by STM32CubeMX : 

void SystemClock_Config (void)
{
 LL_FLASH_SetLatency(LL_FLASH_LATENCY_5);
 while (LL_FLASH_GetLatency() != LL_FLASH_LATENCY_5)
 {
 }

 LL_PWR_SetRegulVoltageScaling(LL_PWR_REGU_VOLTAGE_SCALE0);
 while (LL_PWR_IsActiveFlag_VOS() == 0)
 {
 }
 LL_RCC_HSE_Enable();

 /* Wait till HSE is ready */
 while (LL_RCC_HSE_IsReady() != 1)
 {
 }

 LL_RCC_LSI_Enable();

 /* Wait till LSI is ready */
 while (LL_RCC_LSI_IsReady() != 1)
 {
 }

 LL_RCC_PLL1_SetSource(LL_RCC_PLL1SOURCE_HSE);
 LL_RCC_PLL1_SetVCOInputRange(LL_RCC_PLLINPUTRANGE_2_4);
 LL_RCC_PLL1_SetVCOOutputRange(LL_RCC_PLLVCORANGE_WIDE);
 LL_RCC_PLL1_SetM(12);
 LL_RCC_PLL1_SetN(250);
 LL_RCC_PLL1_SetP(2);
 LL_RCC_PLL1_SetQ(4);
 LL_RCC_PLL1_SetR(2);
 LL_RCC_PLL1P_Enable();
 LL_RCC_PLL1_Enable();

 /* Wait till PLL is ready */
 while (LL_RCC_PLL1_IsReady() != 1)
 {
 }

 LL_RCC_SetSysClkSource(LL_RCC_SYS_CLKSOURCE_PLL1);

 /* Wait till System clock is ready */
 while (LL_RCC_GetSysClkSource() != LL_RCC_SYS_CLKSOURCE_STATUS_PLL1)
 {
 }

 LL_RCC_SetAHBPrescaler(LL_RCC_SYSCLK_DIV_1);
 LL_RCC_SetAPB1Prescaler(LL_RCC_APB1_DIV_1);
 LL_RCC_SetAPB2Prescaler(LL_RCC_APB2_DIV_1);
 LL_RCC_SetAPB3Prescaler(LL_RCC_APB3_DIV_1);
 LL_SetSystemCoreClock(250000000);

 /* Update the time base */
 if (HAL_InitTick(TICK_INT_PRIORITY) != HAL_OK)
 {
 Error_Handler();
 }
}

PLL2 is never init although PLL2Q is selected in USB Clock Mux.

 

3 replies

Technical Moderator
February 26, 2026

Hi @KevinW 

Would you attach your IOC file?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL
KevinWAuthor
Associate
March 7, 2026

Hi @FBL 

Please find the .ioc in attached file.

Also, I configured USB in device mode with default pins (PA11/PA12). Both pins aren't set up, I had to configure them manually (I don't use ST USB Stack but tinyUSB because I need USBTMC class that isn't provided with ST USB stack).

Technical Moderator
March 9, 2026

Hi @KevinW 

Did you check HAL_PCD_MspInit() inside stm32h5xx_hal_msp.c? 

On my side, CubeMX generated it as follows:

void HAL_PCD_MspInit(PCD_HandleTypeDef* hpcd)
{
 if(hpcd->Instance==USB_DRD_FS)
 {
 /* USER CODE BEGIN USB_DRD_FS_MspInit 0 */

 /* USER CODE END USB_DRD_FS_MspInit 0 */
 LL_RCC_SetUSBClockSource(LL_RCC_USB_CLKSOURCE_PLL2Q);

 /* Peripheral clock enable */
 __HAL_RCC_USB_CLK_ENABLE();
 /* USB_DRD_FS interrupt Init */
 HAL_NVIC_SetPriority(USB_DRD_FS_IRQn, 5, 0);
 HAL_NVIC_EnableIRQ(USB_DRD_FS_IRQn);
 /* USER CODE BEGIN USB_DRD_FS_MspInit 1 */

 /* USER CODE END USB_DRD_FS_MspInit 1 */

 }

}

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL