Failure receiving usart signals on one scenario and not the other.
Hey there community,
I am having trouble fixing an interesting scenario on Usart communication,
With the same software doing a reception on a given usart interface, It has been noticed the reception segregates one connection but not the other, Both connections having the same configuration
It has been tested that the board on which it fails has connection on that line and that the connection actually reaches the intended pin for sure by testing the Usart Rx pin when set up as a both a GPIO input and latter as an output.
by playing with this GPIO input and output mechanisms on that pin. and observing respectively from both the led toggles on the board intended to signify sign of life on the pin and, logic analyzer to see the GPIO state when toggled from with in the system.
Note, we are able to see the usart signals on both and are able to decode the messages on a logic analyzer for both, but the stm does not receive the message on one connection.
We appreciate any insight into the Issue