(FD)CAN module resends with ACK visible on bus
Hello everybody,
I am new here so please let me know, if there is important information missing. Thank you already for you time!
I set up a STM32U575I-EV board for communication with CAN. The STM Board, a PCAN-USB dongle and an Oszilloskope are connected to the bus. The Bus is terminated correctly with two 120 Ohm resistors. I use the HAL libraries to interface with the FDCAN peripherie. The jumpers from the eval board are set to connect PB9 and PB8 with the CAN transceiver and to disconnect PB8 from the USB-C PD-interface.
To test the setup I send dummy frames (ID: 0x000, DLC: 1, Data: 0x00). The frame is visible on the Bus and also the ACK from PCAN is visibile. PCAN USB has a 200mV higher voltage on CAN High 0 level.
Here is the dummy frame on the Oszi:

As you see on the the screenshot, the ACK is there and even though I put only one message in the Tx-Buffer of the FDCAN, it retransmitted.
Here is my code:
main.c
int main(void)
{
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the System Power */
SystemPower_Config();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_ADC1_Init();
MX_FDCAN1_Init();
MX_ICACHE_Init();
MX_RTC_Init();
MX_TAMP_RTC_Init();
MX_TSC_Init();
/* USER CODE BEGIN 2 */
//
HAL_FDCAN_Start(&hfdcan1);
while (hfdcan1.State != HAL_FDCAN_STATE_BUSY); /* Wait until FDCAN1 is ready */
while(1) {
uint16_t can_id = 0x000; // Example CAN ID for motor control
uint8_t data[1] = {0x00}; // Example command data
send_CAN_frame(can_id, data, sizeof(data));
FDCAN_ProtocolStatusTypeDef status;
HAL_FDCAN_GetProtocolStatus(&hfdcan1, &status);
FDCAN_ProtocolStatusTypeDef status2 = status; // so status is not optimized out
HAL_Delay(1000);
}
}send_CAN_frame(...) :
void send_CAN_frame(uint16_t id, uint8_t *data, uint8_t length)
{
// Create a CAN message
FDCAN_TxHeaderTypeDef TxHeader;
TxHeader.Identifier = id; // CAN ID
TxHeader.IdType = FDCAN_STANDARD_ID; // 11 Bit ID
TxHeader.TxFrameType = FDCAN_DATA_FRAME; // dataframe
if (length > 8)
length = 8; // Maximal 8 Bytes für Classic CAN
TxHeader.DataLength = length; // 8 Bytes
TxHeader.ErrorStateIndicator = FDCAN_ESI_ACTIVE;
TxHeader.BitRateSwitch = FDCAN_BRS_OFF; // only relevant for FDCAN
TxHeader.FDFormat = FDCAN_CLASSIC_CAN; // Classic CAN
TxHeader.TxEventFifoControl = FDCAN_STORE_TX_EVENTS;
TxHeader.MessageMarker = 0;
HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1, &TxHeader, data)
FDCAN_ProtocolStatusTypeDef status;
HAL_FDCAN_GetProtocolStatus(&hfdcan1, &status);
printf("%lu\n", status.LastErrorCode);
return;
}MX_FDCAN1_Init(...) :
static void MX_FDCAN1_Init(void)
{
hfdcan1.Instance = FDCAN1;
hfdcan1.Init.ClockDivider = FDCAN_CLOCK_DIV1;
hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;
hfdcan1.Init.AutoRetransmission = DISABLE;
hfdcan1.Init.TransmitPause = DISABLE;
hfdcan1.Init.ProtocolException = DISABLE;
hfdcan1.Init.NominalPrescaler = 4;
hfdcan1.Init.NominalSyncJumpWidth = 1;
hfdcan1.Init.NominalTimeSeg1 = 255;
hfdcan1.Init.NominalTimeSeg2 = 64;
hfdcan1.Init.DataPrescaler = 1;
hfdcan1.Init.DataSyncJumpWidth = 1;
hfdcan1.Init.DataTimeSeg1 = 1;
hfdcan1.Init.DataTimeSeg2 = 1;
hfdcan1.Init.StdFiltersNbr = 0;
hfdcan1.Init.ExtFiltersNbr = 0;
hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)
{
Error_Handler();
}
}
"status" from main() gives me a LastErrorCode of Stuff error, Form error and Acknowledge error (0b0..0111).
What I have tried:
- Run release build instead of Debug -> same result
- run FDCAN in external loopback mode -> same result (?!). So the CAN module does resend the frames even though it should ignore ACK errors ( reference manual page 3034)
- When I poll for Rx frames and send frames via PCAN I receive every ~10th frame
Anybody has an idea?