FDCAN Classical STM32G473 not working with canBus
- March 4, 2026
- 2 replies
- 350 views
Hey I am having trouble tryng to connect my stm32g473 to a canbus. I am using a l9616 as a transceiver and the bus is functions as I have connected to it with an stm32f722re with the same l9616.
The clock is 64Mhz,Ive used the canbit time calculation website to define the values of nominal time 1 and 2 to achive 500kbs.
Also using NVIC and it seems to be configured fine. When tested in loopback the interrupt is called and the messages are received.
This is the init with the filter config,as I ve understand I am not filtering anything and any of the messages on the bus should get to my uC.
When running the state of hfdcan1 is Busy and also no error code show up.
FDCAN_HandleTypeDef hfdcan1;
/* FDCAN1 init function */
void MX_FDCAN1_Init(void)
{
/* USER CODE BEGIN FDCAN1_Init 0 */
/* USER CODE END FDCAN1_Init 0 */
/* USER CODE BEGIN FDCAN1_Init 1 */
/* USER CODE END FDCAN1_Init 1 */
hfdcan1.Instance = FDCAN1;
hfdcan1.Init.ClockDivider = FDCAN_CLOCK_DIV1;
hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;
hfdcan1.Init.AutoRetransmission = DISABLE;
hfdcan1.Init.TransmitPause = DISABLE;
hfdcan1.Init.ProtocolException = DISABLE;
hfdcan1.Init.NominalPrescaler = 1;
hfdcan1.Init.NominalSyncJumpWidth = 1;
hfdcan1.Init.NominalTimeSeg1 = 111;
hfdcan1.Init.NominalTimeSeg2 = 16;
hfdcan1.Init.DataPrescaler = 1;
hfdcan1.Init.DataSyncJumpWidth = 1;
hfdcan1.Init.DataTimeSeg1 = 1;
hfdcan1.Init.DataTimeSeg2 = 1;
hfdcan1.Init.StdFiltersNbr = 1;
hfdcan1.Init.ExtFiltersNbr = 0;
hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN FDCAN1_Init 2 */
FDCAN_FilterTypeDef sFilter;
sFilter.IdType = FDCAN_STANDARD_ID;
sFilter.FilterIndex = 0;
sFilter.FilterType = FDCAN_FILTER_MASK;
sFilter.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
sFilter.FilterID1 = 0x000;
sFilter.FilterID2 = 0x000;
if (HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilter) != HAL_OK)
{
Error_Handler();
}
if (HAL_FDCAN_ConfigGlobalFilter(&hfdcan1,
FDCAN_ACCEPT_IN_RX_FIFO0,
FDCAN_ACCEPT_IN_RX_FIFO0,
FDCAN_REJECT_REMOTE,
FDCAN_REJECT_REMOTE) != HAL_OK)
{
Error_Handler();
}
/* USER CODE END FDCAN1_Init 2 */
}Also here is the circuit of the transceiver if that helps,I have 5v stable and gnd on the transceiver itself