Skip to main content
Associate II
June 13, 2025
Solved

FDCAN STM32H753VIT6 – Unable to Achieve >1.92 Mbps Data Rate (PLL1Q = 40 MHz)

  • June 13, 2025
  • 2 replies
  • 1493 views

Hi ST Community,

I’m working on a CAN FD project using the STM32H753VIT6 and facing a limitation with data phase bitrate while using Bit Rate Switching (BRS).

My Setup:

  • Controller: STM32H753VIT6

  • FDCAN clock source: PLL1Q

  • PLL1Q output: 40 MHz

  • Frame format: CAN FD with BRS (FDCAN_FRAME_FD_BRS)

  • Nominal (arbitration) bitrate: 1 Mbps

  • Target data bitrate: 2 Mbps or higher

     Problem:

    Despite the configuration, I'm not able to achieve more than ~1.92 Mbps on the data phase. Even when I reduce the number of time quanta or adjust prescalers, the speed does not increase beyond this limit.

     My Questions:

    1. Is there any known limitation when using PLL1Q = 40 MHz for FDCAN clock?

    2. Is the STM32H753 internal FDCAN limited to certain bitrates per kernel clock frequency?

    3. Could internal synchronization or sampling constraints prevent achieving the expected 2.5 Mbps from a 40 MHz FDCAN clock?

      Attachments:

      • main.c file

      • Oscilloscope screenshot showing BRS waveform and time base

      • STM32CubeMX clock configuration screenshot

    Any insights or suggestions would be greatly appreciated!

    Thanks in advance,
    Pavan

Best answer by mƎALLEm

Did you activate the delay compensation?:

 /**
 * Configure and enable Tx Delay Compensation, required for BRS mode.
 * TdcOffset default recommended value: DataTimeSeg1 * DataPrescaler
 * TdcFilter default recommended value: 0
 */
 if (HAL_FDCAN_ConfigTxDelayCompensation(&hfdcan1, (hfdcan1.Init.DataPrescaler * hfdcan1.Init.DataTimeSeg1), 0U) != HAL_OK)
 {
 Error_Handler();
 }

 if (HAL_FDCAN_EnableTxDelayCompensation(&hfdcan1) != HAL_OK)
 {
 Error_Handler();
 }

Please refer to this Github link linked to this article: STM32 FDCAN running at 8 Mb/s on NUCLEO boards

 

2 replies

mƎALLEm
Technical Moderator
June 13, 2025

Hello,

I don't think there is a limitation 40Mhz vs bitrate > 2Mb/s

Refer to this article: STM32 FDCAN running at 8 Mb/s on NUCLEO boards on which we showed that we can reach 8Mb/s in data phase.

Check also your transceiver bandwidth.

Meanwhile refer to this article: FAQ: Fixing STM32 FDCAN communication disruptions - APB bus, kernel, and time quanta clocks and check if you are in the same situation

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
pavanlAuthor
Associate II
June 13, 2025

Thank you for your response.

My transceiver bandwidth is 5 MHz for FDCAN and 1 MHz for classic CAN.

I followed the same clock configuration as mentioned, but I'm still unable to achieve a speed beyond 2 Mbps. Could you please suggest the best approach to troubleshoot this issue? If there’s a possibility of any mistake in my configuration or code, I would really appreciate your guidance.

Thanks again.

mƎALLEm
Technical Moderator
June 13, 2025

Were you able to achieve the target bitrate in Loopback mode?

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
MHoll.2
Senior III
June 15, 2025

I think You have set the Data baudrate wrong. If You have set the FDCAN Clock to 50MHz then Your setup:

 hfdcan1.Init.NominalPrescaler = 1;
 hfdcan1.Init.NominalSyncJumpWidth = 4;
 hfdcan1.Init.NominalTimeSeg1 = 86;
 hfdcan1.Init.NominalTimeSeg2 = 13;
 hfdcan1.Init.DataPrescaler = 1;
 hfdcan1.Init.DataSyncJumpWidth = 2;
 hfdcan1.Init.DataTimeSeg1 = 10;
 hfdcan1.Init.DataTimeSeg2 = 2;

will result in:

Nominal Bitrate: 50e6/(1+86+13) = 500e3 (500kBit)

Data Bitrate: 50e6/(1+10+2) = 3.8462e6(!)

if You want 500KBit/2Mbit You have to cange the Data segment's (for example 20 and 4)

pavanlAuthor
Associate II
June 19, 2025

i already set this with 50 MHz. but I don't get more than 1.92 mbps"

pavanl_0-1750323892090.png

 

mƎALLEm
Technical Moderator
June 19, 2025

You didn't answer that question: did you try with the Loopback mode?

 

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."