Skip to main content
labrat0638
Associate
December 19, 2025
Solved

H755 - STLink Virtual com port do not appear in Windows 10 Device Manager but it does on other Windows 11 machine

  • December 19, 2025
  • 1 reply
  • 459 views

Hi, I'm currently working on a project with an H755 board.

The project uses UART communication.
I'm developing it on a Windows 11 computer, and it generally works fine on that computer. So far, there are no issues.

However, after completing the project, I'd like to be able to use it on my older laptop (currently running Windows 10 with ESU).
Here's the problem: my Windows 10 computer doesn't recognize the STLink virtual COM port. It only sees the device as a standard COM port with a Microsoft driver (not ST Microelectronics), and its UART communication then doesn't work.

I don't have CubeIDE installed on my laptop.
I don't need it on this computer. Should I install the driver manually? If so, where can I find it? Any ideas on how to solve this problem?

Best answer by TDK

Worth a shot:

STSW-LINK009 | Software - STMicroelectronics

 

1 reply

TDK
TDKBest answer
Super User
December 19, 2025
"If you feel a post has answered your question, please click ""Accept as Solution""."
labrat0638
Associate
December 19, 2025

Thankst, this is exactly what I needed. Now works fine on older machine.