H7x3: SDMMC2 - no DMA?
Heyho,
I just changed a big PCB (1st revision working) with a H733 and added a micro SD cardholder and connected it to the SDMMC2 peripheral.
Only to find out later that this #2 does NOT work with the extra IDMA controller.
SDMMC1 is out of the question because I absolutely need I2SCKIN for the SAIs, and I didn't want to change the complete pin-out and PCB design (Altium says: Components on board: 1015).
I'm pretty sure I've checked the RM, but maybe I oversaw something...
So, is there any way to use another DMA with SDMMC2 ?
Thanks in advance!