Skip to main content
Associate
January 10, 2026
Question

Hello World Error Program

  • January 10, 2026
  • 2 replies
  • 366 views

I have a problem, where there's simply no error, but the output, is not showing on the screen. The system has detected the board, and all the correct steps are followed, even though, my hello world code is not been printed. I am using stm32cubeide version 2.0.0 and im using a nucleo-h723zg. Also, the board is first showing a static red light when plugegd in to the laptop, and then a patternt that repeats ----> red, green red,green and then green for 1 second and then it keeps on going. I even flashed my whole baord and erased everything, despite that, it is showing the same behaviour. So far, I haven't recieved any error, the only thing is that i am not able to see the output on the screen of the ide that im using.  Here's a link for the led problem(chatgpt says its a firware issue evn though i downlaoded the correct firmware) 

Video link: https://youtube.com/shorts/vETuGu5Kbfg?feature=share

2 replies

Pavel A.
Super User
January 11, 2026

The blinking red/green LED shows activity of the ST-LINK on the board, this is normal, not any error.

Your program does not print anything because the Nucleo has no printer and no screen :) You can only print to the UART connected to the "virtual com port" of the ST-LINK, or thru ITM interface. Both ways can be displayed in CubeIDE, but differently. What is your choice?

Don't take chatgpt too seriously, sometimes it just hallucinates.

 

 

 

Mohit79Author
Associate
January 11, 2026

Thank you for your reply! actually, i want to take inputs of the nucelo board to my cubeide ver. 2.0.0 and want to display it on the port 0. I know nucleo dosent have any screen/printer :) but i want to display it n my laptops cubeide thru ST-LINK my currecnt setup is htat ive connected my nucleo board to my laprop with a usb cable and I chose the SWD interface and my Core clock is set to 400, i even tried 64 (MHz) as the board is, and also the SWO to 2000 (KHz) as per my instructor, im only using ITM interface and no uart interface :)

Aand yes i know chatgpt just sometimes blabbers things as it dosent have anything to say and i have to admit its not that helpful lol :) thank you so much for your help! 

Pavel A.
Super User
January 11, 2026

Hi,

Please read carefully the CubeIDE user guide, it explains the how to's. The ITM can be a bit tricky. Sometimes it takes several restarts of the program to get it working. Of course assuming that the code is correct, with all the _write etc. patches.

Note that the CoreClock will be 400 MHz only if you use PLL clock with HSE, and after SystemClock_Config call. Do not print before SystemClock_Config returns.