Skip to main content
Visitor II
April 9, 2024
Question

High current consumption in Stop Mode on STM32U575 DEV Kit and Custom Board

  • April 9, 2024
  • 1 reply
  • 1585 views

Hi,

I'm currently debugging what I think to be a code issue. I have a custom board with all peripherals physically disconnected and a NUCLEO-U575ZI-Q dev kit. The lowest current I see is about 250uA on both setups, with a sawtooth charge/discharge waveform from what I think is the internal switching regulator (consistent when using other stop mode functions). I've implemented a few examples for entering stop mode, and review any application notes I could find for how to handle it. Stop1 and Stop2 both yield current in the ~200uA range, and Stop3 yields about 35uA. The only way I have found to decrease the current the most were changing the "PWR_CR1_LPMS_X" parameters in the HAL_PWREx_EnterSTOP1Mode function:

Original: MODIFY_REG(PWR->CR1, PWR_CR1_LPMS, PWR_CR1_LPMS_0);
New 1: MODIFY_REG(PWR->CR1, PWR_CR1_LPMS, PWR_CR1_LPMS_1); -> Gave me <200uA on my custom board
New 2: MODIFY_REG(PWR->CR1, PWR_CR1_LPMS, PWR_CR1_LPMS_2); -> Gave me 90uA on my custom board

Changing the LPMS bit to 1 or 2 gets rid of the sawtooth waveform, but I know these bits depending on the Stop mode, so it's strange that setting a different LPMS bit eliminates that behavior?

Here is my function that handles entering Stop1:

DBGMCU->CR = 0;

RCC_OscInitTypeDef RCC_OscInitStruct;
/* Disable HSI oscillator */
// May or may not be shut off automatically depending on peripheral configuration. This ensures its off

RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_OFF;


GPIO_InitTypeDef GPIO_InitStruct;
// Put all GPIOs into analog state
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
__HAL_RCC_GPIOE_CLK_ENABLE();
__HAL_RCC_GPIOF_CLK_ENABLE();
__HAL_RCC_GPIOG_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOI_CLK_ENABLE();

// Set parameters to be configured

GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Pin = GPIO_PIN_ALL;

/* Initialize all GPIO pins */

HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);
HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);
HAL_GPIO_Init(GPIOH, &GPIO_InitStruct);
HAL_GPIO_Init(GPIOI, &GPIO_InitStruct);

/* Disable all GPIO clocks */

__HAL_RCC_GPIOA_CLK_DISABLE();
__HAL_RCC_GPIOB_CLK_DISABLE();
__HAL_RCC_GPIOC_CLK_DISABLE();
__HAL_RCC_GPIOD_CLK_DISABLE();
__HAL_RCC_GPIOE_CLK_DISABLE();
__HAL_RCC_GPIOF_CLK_DISABLE();
__HAL_RCC_GPIOG_CLK_DISABLE();
__HAL_RCC_GPIOH_CLK_DISABLE();
__HAL_RCC_GPIOI_CLK_DISABLE();

HAL_ADC_DeInit(&hadc1);

if(huart2.gState != HAL_UART_STATE_RESET)
HAL_UART_DeInit(&huart2);

if(huart3.gState != HAL_UART_STATE_RESET)
HAL_UART_DeInit(&huart3);

if(huart4.gState != HAL_UART_STATE_RESET)
HAL_UART_DeInit(&huart4);

if(huart5.gState != HAL_UART_STATE_RESET)
HAL_UART_DeInit(&huart5);

if(hlpuart1.gState != HAL_UART_STATE_RESET)
HAL_UART_DeInit(&hlpuart1);

HAL_SuspendTick();

__HAL_RCC_PLL_DISABLE();

HAL_PWREx_EnterSTOP1Mode(PWR_STOPENTRY_WFI);

HAL_PWREx_EnterSTOP1Mode(PWR_STOPENTRY_WFI)

/* Check the parameters */
assert_param(IS_PWR_STOP_ENTRY(STOPEntry));

/* Stop 1 mode */
MODIFY_REG(PWR->CR1, PWR_CR1_LPMS, PWR_CR1_LPMS_0);

/* Set SLEEPDEEP bit of Cortex System Control Register */
SET_BIT(SCB->SCR, ((uint32_t)SCB_SCR_SLEEPDEEP_Msk));

/* Select Stop mode entry */
if (STOPEntry == PWR_STOPENTRY_WFI)
{
/* Request Wait For Interrupt */
__WFI();
}
else
{
/* Request Wait For Event */
__SEV();
__WFE();
__WFE();
}

/* Reset SLEEPDEEP bit of Cortex System Control Register */
CLEAR_BIT(SCB->SCR, ((uint32_t)SCB_SCR_SLEEPDEEP_Msk));

I've also probed every pin on my MCU to see if there's still some leakage, and I didn't see any improvement. It seems like there's something wrong with the firmware

1 reply

ST Employee
April 15, 2024

Hi @mrask 

Thank you for the content furnished in your post. In RM0456, page 440, you have all the different values possible for LPMS.

AlexisL_0-1713187508307.png

The function HAL_PWREx_EnterSTOP1Mode is using the MODIFY_REG macro, which clears LPMS and set the bit LPMS0. That, way, LPMS value is now 001, or STOP1 mode.

If you want to lower your power consumption, you have to change the LPMS register value as you did, or you can use the following available functions:

  • HAL_PWREx_EnterSTOP2Mode 
  • HAL_PWREx_EnterSTOP3Mode 
  • HAL_PWR_EnterSTANDBYMode
  • HAL_PWREx_EnterSHUTDOWNMode

 

Attention 1: Stop 3 mode is actually quite different, please read Tables 99 and 100 in order to check the compliancy with your application.

Attention 2: Standby and Shutdown mode will trigger an internal hardware reset during the wake up.

 

Hope this will help you.
Best regards,

___________________________________________________________________________________________

Alexis LOUIS
ST Embedded Software Engineer

Visitor II
June 12, 2025

I am having similar problem with U575. When I load new firmware with STcube programmer and let it run when it goes into STOP2 mode it draws about 1ma. If I soft reset or hard reset it starts up with same 1ma STOP2 current. If I power off/on same firmware STOP2 current is 200ua after which a soft or hard reset will stay at 200ua. What is being initialized by power off/on that hard or soft reset does not do. I notice the same issue if I OTA (cellular) the same firmware without a power off/on and only soft reset it goes to 1ma and not to lower 200ua STOP2 current. I also noticed that when replacing the L496 with U575 running very close to same firmware my STOP2 current on L496 (including some other leakage on PCB) is 25ua where as same PCB with U575 is 200ua. I tried clearing all bits in RCC regs but no change.