How to backup/restore value of variables in STM32N6570-DK board
Hello,
I have some setup variables in my app which should retained while the power is switched off. Normally I would use the dedicated Backup RAM, but the board does not have backup battery, battery socket, not a battery connector. The Backup RAM is not usable with STM32n6570-DK board.
The MCU does not have internal flash memory with backup area. (This worked with H747 and H723 MCUs) The board has an external 1Mbit flash memory controlled by OCTOSPI so I might store data in the external flash. I need max 512 bytes only. This 512-byte backup should be placed to the end of the external flash.
Can anybody advice how to do this?
Best regards,
Louis