Skip to main content
Associate III
July 23, 2025
Solved

How to configure multiple ADC channel with interrupt mode? STM32L0

  • July 23, 2025
  • 1 reply
  • 412 views

Hi all,

I have two ADC channels (channel 1 and channel 3), and I configured them in multi-channel interrupt mode. 

The cubeMx ADC settings is shown in image below:

Continuous Convertion mode : Enabled

End of Conversion Selection: End of single convertion

 

chai2145_0-1753238715037.png

 

chai2145_2-1753238860394.png

 

However, when the interrupt is triggered and I read both channel values, the readings are incorrect. Specifically, the value from channel 1 appears to be assigned to both variables, even though only channel 1 was triggered.

 

Code:

 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2025 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "stdio.h"
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_ADC_Init(void);
/* USER CODE BEGIN PFP */
volatile uint16_t g_adcVal[2] = {0};
volatile static uint8_t g_adcIndex = 0;
/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc)
{
	// Read latest converted value
	g_adcVal[g_adcIndex] = HAL_ADC_GetValue(hadc);

	// Move to next channel
	g_adcIndex++;
	if (g_adcIndex >= 2)
	{
		g_adcIndex = 0;
	}
}

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_ADC_Init();
 /* USER CODE BEGIN 2 */
 // Start ADC Conversion
 HAL_ADCEx_Calibration_Start(&hadc, ADC_SINGLE_ENDED); // Calibrate The ADC On Power-Up For Better Accuracy
 HAL_ADC_Start_IT(&hadc);

 	// Start timer to trigger ADC, sampling rate at 100Hz
 	//HAL_TIM_Base_Start(&htim6);
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
	 printf("test\n");
	 printf("adc1:%d",g_adcVal[0]);
	 printf("adc2:%d",g_adcVal[1]);
	 HAL_Delay(1000);
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI;
 RCC_OscInitStruct.MSIState = RCC_MSI_ON;
 RCC_OscInitStruct.MSICalibrationValue = 0;
 RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_5;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief ADC Initialization Function
 * None
 * @retval None
 */
static void MX_ADC_Init(void)
{

 /* USER CODE BEGIN ADC_Init 0 */

 /* USER CODE END ADC_Init 0 */

 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC_Init 1 */

 /* USER CODE END ADC_Init 1 */

 /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
 */
 hadc.Instance = ADC1;
 hadc.Init.OversamplingMode = DISABLE;
 hadc.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
 hadc.Init.Resolution = ADC_RESOLUTION_12B;
 hadc.Init.SamplingTime = ADC_SAMPLETIME_160CYCLES_5;
 hadc.Init.ScanConvMode = ADC_SCAN_DIRECTION_FORWARD;
 hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc.Init.ContinuousConvMode = ENABLE;
 hadc.Init.DiscontinuousConvMode = DISABLE;
 hadc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc.Init.DMAContinuousRequests = DISABLE;
 hadc.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc.Init.LowPowerAutoWait = DISABLE;
 hadc.Init.LowPowerFrequencyMode = ENABLE;
 hadc.Init.LowPowerAutoPowerOff = DISABLE;
 if (HAL_ADC_Init(&hadc) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure for the selected ADC regular channel to be converted.
 */
 sConfig.Channel = ADC_CHANNEL_1;
 sConfig.Rank = ADC_RANK_CHANNEL_NUMBER;
 if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure for the selected ADC regular channel to be converted.
 */
 sConfig.Channel = ADC_CHANNEL_3;
 if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC_Init 2 */

 /* USER CODE END ADC_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 /* USER CODE BEGIN MX_GPIO_Init_1 */

 /* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOA_CLK_ENABLE();

 /* USER CODE BEGIN MX_GPIO_Init_2 */

 /* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * file: pointer to the source file name
 * line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

Results:

chai2145_3-1753239061068.png

 

Does anyone know what happened? Could there be a misconfiguration in my ADC settings?

 

Thanks

 

 

Best answer by TDK

If you run the code without breaking, what story do the printf statements tell?

It could be that the ADC is being overran because it isn't serviced frequently enough. Pausing in the debugger is sure to mess with things. Consider reading the OVR flag to see if this is happening. Otherwise things look correct.

For this reason, it is typically better to use DMA when converting multiple channels.

1 reply

TDK
TDKBest answer
Super User
July 23, 2025

If you run the code without breaking, what story do the printf statements tell?

It could be that the ADC is being overran because it isn't serviced frequently enough. Pausing in the debugger is sure to mess with things. Consider reading the OVR flag to see if this is happening. Otherwise things look correct.

For this reason, it is typically better to use DMA when converting multiple channels.

"If you feel a post has answered your question, please click ""Accept as Solution""."
chai2145Author
Associate III
July 23, 2025

Hi TDK, 

The values appear to be correct when printed over the serial interface!! Thank you. 

Sorry to ask and don't know this phenomenon, we are not supposed to break into or debug the ISR because pausing in the debugger will mess things up? Then how do we debugging the ISR?

 

chai2145_0-1753241491225.png

 

TDK
Super User
July 23, 2025

 

I would suggest using DMA to convert multiple channels, or to use a timer to trigger ADC conversions and have the timer frozen when the core is halted.

"If you feel a post has answered your question, please click ""Accept as Solution""."