Skip to main content
Associate II
February 8, 2024
Question

How to detect if usb connection is established

  • February 8, 2024
  • 5 replies
  • 7147 views

Hey. I'm trying to use my H7's usb interface and i've currently set it up as a cdc device.
What i'm trying to implement though is the following. 

The stm is supposed to create a virtual connection with either a python app or a tera term terminal.

Is there a function or a variable that detects if this kind of a connection is established ? For example, the pico equivalent is tud_cdc_connected()

 What i want to build is this

while(!exampleCOnnectionVariable)
{
 HAL_DELAY(500)
}

Meaning that my stm would wait during initialization, until a connection is established and then proceed with the super loop.

5 replies

gbm
Principal
February 8, 2024

With classic ST USB stack, you need to implement CDC_SET_CONTROL_LINE_STATE request in usbd_cdc_if.c. When ControlLineState value changes from anything different from 3 to 3, the connection is established. You may start transmitting data no sooner than 50 ms after that change.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
TDK
Super User
February 8, 2024

Check dev_state for configured status.

if (hUsbDeviceFS.dev_state == USBD_STATE_CONFIGURED) {
 ...
}

 

This doesn't mean the program has the port open, just that the computer is connected. No way to detect when a program opens the serial port.

"If you feel a post has answered your question, please click ""Accept as Solution""."
gbm
Principal
February 8, 2024

dev_state remains at CONFIGURED even after you disconnect the USB cable...

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
TDK
Super User
February 9, 2024

If your device is bus-powered, disconnecting the cable stops the program. No problems there.

If your device is self-powered, you are required (per USB standard) to monitor VBUS and de-initialize the peripheral when VBUS drops by calling MX_USB_DEVICE_DeInit(). This will reset the state machine back to USBD_STATE_DEFAULT.

Edit: If you ignore the standard, there's probably a state variable you could check somewhere. I may look into it.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Technical Moderator
February 8, 2024

Hello @AlexandrosAA 

If I understand your request correctly, in usbd_conf.c, you can check device connection from ISR through USBD_LL_DevConnected in callback.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL
Associate II
February 9, 2024

I tried something like this

while(CDC_Transmit_HS(messageOk,sizeof(messageOk))!=USBD_OK)
{

}

but it seems that the message is transmitted, even if the port is not open. Is there a similar approach to this ? The while loop should end only if the data are accepted by my computer.

Technical Moderator
February 9, 2024

@AlexandrosAA When stepping in debug, and you reach this line as previously mentioned.

if (hUsbDeviceFS.dev_state == USBD_STATE_CONFIGURED) {

 You are pretty sure your host is connected.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL
Visitor II
April 2, 2025

Here is the solution I found. It blocks execution until a terminal is connected (DTR on). It also includes a fix for Windows, where the Virtual COM port doesn’t work.

File `main.c`

 /* USER CODE BEGIN 2 */
 while (CDC_Get_DTR_State() == 0) {
	 HAL_Delay(10); // Wait 10 ms before re-check
 }
 /* USER CODE END 2 */

File `usbd_cdc_if.h`

/* USER CODE BEGIN EXPORTED_FUNCTIONS */
uint8_t CDC_Get_DTR_State(void);
uint8_t CDC_Get_RTS_State(void);
/* USER CODE END EXPORTED_FUNCTIONS */

File `usbd_cdc_if.c`

/* USER CODE BEGIN PV */
/* Private variables ---------------------------------------------------------*/
// For the CDC driver to work on Windows
USBD_CDC_LineCodingTypeDef LineCoding =
{
		115200, /* baud rate */
		0x00, /* stop bits-1 */
		0x00, /* parity - none */
		0x08 /* nb. of bits 8 */
};

volatile uint8_t dtr_state = 0; // Global variable to store DTR state
volatile uint8_t rts_state = 0; // Global variable to store RTS state
/* USER CODE END PV */

...

static int8_t CDC_Control_FS(uint8_t cmd, uint8_t* pbuf, uint16_t length)
{
 /* USER CODE BEGIN 5 */
 switch(cmd)
 {
 case CDC_SEND_ENCAPSULATED_COMMAND:

 break;

 case CDC_GET_ENCAPSULATED_RESPONSE:

 break;

 case CDC_SET_COMM_FEATURE:

 break;

 case CDC_GET_COMM_FEATURE:

 break;

 case CDC_CLEAR_COMM_FEATURE:

 break;

 /*******************************************************************************/
 /* Line Coding Structure */
 /*-----------------------------------------------------------------------------*/
 /* Offset | Field | Size | Value | Description */
 /* 0 | dwDTERate | 4 | Number |Data terminal rate, in bits per second*/
 /* 4 | bCharFormat | 1 | Number | Stop bits */
 /* 0 - 1 Stop bit */
 /* 1 - 1.5 Stop bits */
 /* 2 - 2 Stop bits */
 /* 5 | bParityType | 1 | Number | Parity */
 /* 0 - None */
 /* 1 - Odd */
 /* 2 - Even */
 /* 3 - Mark */
 /* 4 - Space */
 /* 6 | bDataBits | 1 | Number Data bits (5, 6, 7, 8 or 16). */
 /*******************************************************************************/
 case CDC_SET_LINE_CODING:
 	LineCoding.bitrate = (uint32_t)(pbuf[0] | (pbuf[1] << 8) | (pbuf[2] << 16) | (pbuf[3] << 24));
 	LineCoding.format = pbuf[4];
 	LineCoding.paritytype = pbuf[5];
 	LineCoding.datatype = pbuf[6];
 	break;

 case CDC_GET_LINE_CODING:
 	pbuf[0] = (uint8_t)(LineCoding.bitrate);
 	pbuf[1] = (uint8_t)(LineCoding.bitrate >> 8);
 	pbuf[2] = (uint8_t)(LineCoding.bitrate >> 16);
 	pbuf[3] = (uint8_t)(LineCoding.bitrate >> 24);
 	pbuf[4] = LineCoding.format;
 	pbuf[5] = LineCoding.paritytype;
 	pbuf[6] = LineCoding.datatype;
 	break;

 case CDC_SET_CONTROL_LINE_STATE:
 	// DTR is in bit 0 (LSB) of first byte
 	dtr_state = pbuf[0] & 0x01; // Bit 0 = DTR
 	rts_state = (pbuf[0] & 0x02) >> 1; // Bit 1 = RTS
 break;

 case CDC_SEND_BREAK:

 break;

 default:
 break;
 }

 return (USBD_OK);
 /* USER CODE END 5 */
}

...

/* USER CODE BEGIN PRIVATE_FUNCTIONS_IMPLEMENTATION */
uint8_t CDC_Get_DTR_State(void) {
	return dtr_state;
}

uint8_t CDC_Get_RTS_State(void) {
	return rts_state;
}
/* USER CODE END PRIVATE_FUNCTIONS_IMPLEMENTATION */
Associate II
December 13, 2025

@overlaine thanks for sharing your solution. Could you please specify more detail about "the Virtual COM port doesn’t work in windows", I wonder if we encountered same problem of a serious bug in usbser.sys.

Visitor II
December 14, 2025

Hello,

From what I remember (as this goes back several years), the serial port was correctly enumerated under Windows, but communication between the devices (the PC and the MCU) did not work.
I tested it again today without the fix, and it now works under Windows.

Most likely this is due to a driver update, if I am to believe this post:
post_link