Skip to main content
tmuyesmu
Associate
December 2, 2013
Question

How to setup SPI interrupt on STM32F4 slave?

  • December 2, 2013
  • 1 reply
  • 692 views
Posted on December 02, 2013 at 13:59

Hi, can someone point me in the right direction/instructions/tutorials on how to setup an interrupt on a STM32F4 as a slave that would trigger when an STM32F4 master sends data?

Do i just need to set up the NVIC on the slave device or would I also need to set up interrupts from the master?

#stm32f4-spi-interrupt
This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
December 2, 2013
Posted on December 02, 2013 at 15:53

All behaviour related to the slave would need to be coded on the slave side. Set up the SPI Interrupt in the NVIC, and enable the RXNE interrupt, and TXE if appropriate, and perhaps an EXTI related to a Chip Select, again if appropriate.

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..