Insights on possible values for ADC input voltage swing using external VREF
Hello Community,
We are designing a simply cost sensitive Temperature sensing solution using low-cost Linear Thermistors TMP61Q1 from TI, and wish to use the internal ADCs on STM32G474RCT3 MCUs, this is an LQFP64 package with a dedicated VREF Buffer Pin which can drive output loads at 2.048V, 2.5V, 2.9V with 6.5mA.
We wish to understand in detail, can we use this VREF BUFF pin and add an external voltage reference of say 1V & then reduce the ADC input voltage swing to 0-1V for the entire 12-bit dynamic range?
Or can we set the VREF Buffer to 2.048V & use the ADC with VREF Internal channel such that the ADC Voltage swing becomes 0 to 2.048V for entire 12-bit range?
Or can we simply supply VDDA 1V & keep the ADC maximum voltage swing between 0 to 1V for the entire 12-bit resolution?

Kindly guide us with this use case, as the sensor output has a limited voltage swing & using a non-inverting amplifier is not a feasible option cost-wise.
Both I & my team are fairly new to the Analog circuit design & are looking forward for a good starting point to understand the ADCs on STM32G474 from the community.
Regards