Skip to main content
Visitor II
April 20, 2026
Question

Interfacing a 5 V USB Barcode Scanner with STM32F401RE

  • April 20, 2026
  • 2 replies
  • 101 views

Hello everyone,

I am working on a design using STM32F401RE and need to interface a barcode scanner that works over a standard 5 V USB interface.

The barcode scanner behaves like a typical USB device (likely HID/CDC) and expects:

  • USB host on the other end
  • 5 V VBUS supply

it also has RS232 interfacing option aswell.

However, as per STM32F401RE documentation, it supports only VBUS voltage max 3.6V.

I would like guidance on:

  1. Whether it is technically possible to interface a 5 V USB barcode scanner directly with STM32F401RE.
  2. If not, what practical alternatives are recommended.

The goal is to reliably read barcode data into the MCU in an embedded system (no PC involved).

Thanks in advance for your support.

2 replies

Technical Moderator
April 20, 2026

Hi @karan_t 

When STM32 is configured as host you need to configure a pin as output to power the device. You can use one of our reference boards schematics as reference. 

FBL_0-1776678574045.png

 

Caution: Voltage on all STM32 pins must not exceed 4V against VDD, even when the MCU is not powered. 

For the barcode scanner used, check whether it is bus or self powered, and provide the appropriate power supply/sensing accordingly. 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL
Andrew Neil
Super User
April 20, 2026

USB is always 5V !

Take a look at Application Note AN4879, Introduction to USB hardware and PCB guidelines using STM32 MCUs:

AndrewNeil_0-1776680521127.png

https://www.st.com/resource/en/application_note/an4879-introduction-to-usb-hardware-and-pcb-guidelines-using-stm32-mcus-stmicroelectronics.pdf#page=15

 


@karan_t wrote:

it also has RS232 interfacing option as well


Sounds like that would be the easiest option for you!

Are you sure it's actual RS232 - not just TTL ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.