Question
Is it normal if MCU of NUCLEOH743 gets hot at 400/480Mhz and ~120mA current at IDD Jumper?
I am using latest CubeMx and CubeH7 versions
With the increase in clock the MCU start getting hot especially at 400 or 480Mhz. So Is it a normal?
I have also checked the current consumption at IDD jumper and it is ~120mA. Iis this normal value when no external component is attached, default peripherals are configured using CubeMX, 2 LEDs are blinking and clock is 400Mhz?