Skip to main content
Senior
November 12, 2025
Solved

ISR memory update & Timer trigger

  • November 12, 2025
  • 2 replies
  • 181 views

Hello All, 

I am facing a strange situation

I have an ISR function1 that is triggered on Falling / Rising Edge of a GPIO pin 

This function1 according to the state of variable will either start TIMER2 and stop TIMER3 and the way around.

TIMER2 & 3 have also ISR. 

But before starting/stopping TIMER, it needs to update memory variable that will be used by TIMER ISR.

The issue is that the variable is effectively updated in memory after the start of TIMER and a few (100 CPU) cycles are needed to get the proper value.

This is time critical and I need the value of wrBitPos to be 0 and wrBitCounter to be set a the right value before the first timer iteration. 

How can I fix this ?

I use the volatile declaration for variable.

void function1(){
 TIM3->DIER &= ~TIM_DIER_CC4IE; // disable CC4 interrupt
 TIM3->CCER &= ~TIM_CCER_CC4E; // disable CC4 output
 TIM3->CR1 &= ~TIM_CR1_CEN; // stop the timer

 wrBitPos=0; 
 bytePtr++; // Reset the BitPos
 wrBitCounter=bytePtr*8;
 
 TIM2->DIER |= TIM_DIER_CC2IE; // enable CC3 interrupt
 TIM2->CCER |= TIM_CCER_CC3E; // enable CC3 output
 TIM2->CR1 |= TIM_CR1_CEN; // start the 
 

 

Thanks

Vincent 

Best answer by TDK

You can use a data-sync barrier instruction to ensure data written is completed before the CPU moves on. Variables should be marked as volatile as well.

__DSB();

2 replies

TDK
TDKBest answer
Super User
November 12, 2025

You can use a data-sync barrier instruction to ensure data written is completed before the CPU moves on. Variables should be marked as volatile as well.

__DSB();

"If you feel a post has answered your question, please click ""Accept as Solution""."
vbessonAuthor
Senior
November 13, 2025

thanks, precise, clear ! and working