MX25UM51245G not being initialized by bootrom
We are currently working with a custom PCB using an STM32N6 chip and an MX25UM512G flash chip. The flash is connected identically to the Nucleo development board.
When powering up the board in Dev Boot mode, it is not possible to read the flash chip using CubeProgrammer. The MCU crashes, which we assume based on the reduced power consumption observed afterward.
If we first load a firmware image into SRAM using CubeIDE (which successfully connects to and reads the flash memory), then reading and writing the flash via CubeProgrammer works as expected.
However, after a power cycle without reloading the firmware into SRAM, the flash becomes inaccessible again.
Additionally, after flashing the firmware using this workaround (i.e., initializing the flash via our own firmware and then booting in Flash mode), the software is not executed from flash and the system does not boot.
Our assumption is that the flash is not correctly initialized by the boot ROM. Any help or suggestions would be highly appreciated.