N6 PLL: FRAC change on the fly as in H7 impossible ?
Heyho,
the title says it...
In RM0486, 14.6.5 PLL description, page 437 / 438 I find this:
Using the PLLs in fractional mode
PLL off ... set FRAC ... PLL on
Caution: Do not update DIVN and DIVNFRAC after the PLL has been enabled.
On the other hand, there are comments that some dividers can be changed on the fly.
So maybe it might work? Has anybody tried?
With these 4 PLLs and the great clock routing possibilities, the ability to change FRAC values on the fly with this high resolution would be a fantastic feature for synchronization, without using an external VCO.