Skip to main content
This topic has been closed for replies.

28 replies

waclawek.jan
Super User
February 12, 2014
Posted on February 12, 2014 at 14:57

RM0090 rev.6 is out.

Uwe Bonnes
Chief
February 12, 2014
Posted on February 12, 2014 at 16:16

> RM0090 rev.6 is out.

Is there any chance that ST gets their document system a little more sane like:

- provide date of last release on the website.

- not to use 4 names for the same document.

Tesla DeLorean
Guru
February 12, 2014
Posted on February 12, 2014 at 18:45

The use of RM0090 has been pretty consistent. There are dozens of Data Sheet/Manuals for specific part designations.

The site is a bit of an unmanageable train wreck.
Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User
February 12, 2014
Posted on February 12, 2014 at 19:00

>> - not to use 4 names for the same document.

> The use of RM0090 has been pretty consistent.

I believe Uwe meant the fact that for example RM0090 goes under the DM00031020.pdf filename, and is labelled on the pages' footer as Doc ID 018909. This is similar for the other published materials.

JW

waclawek.jan
Super User
May 23, 2014
Posted on May 23, 2014 at 17:24

RM0090 rev.7 is out.

waclawek.jan
Super User
December 1, 2014
Posted on December 01, 2014 at 09:41

RM0090 rev.8 is out.

waclawek.jan
Super User
March 30, 2015
Posted on March 30, 2015 at 12:38

RM0090 rev.9 is out.

waclawek.jan
Super User
August 13, 2015
Posted on August 13, 2015 at 12:29

RM0090 rev.10 is out.

waclawek.jan
Super User
October 29, 2015
Posted on October 29, 2015 at 18:12

RM0090 rev.11 is out.

Datasheet for STM32F40x is in it new rev.6 too. I did not check for other STM32F4xx, but I assume they have new revisions of datasheets too. An interesting detail, reflected both in the datasheet and RM0090 is that the allowed range for PLLs output is now extended downwards to 100MHz. Strangely, the datasheet states the same power consumption at this frequency as it used to be for the significantly higher 192MHz... Could somebody from ST comment on this, please?

JW
Amel NASRI
Technical Moderator
November 9, 2015
Posted on November 09, 2015 at 10:35

Hi waclawek.jan,

To answer you question: We just improved the PLL VCO characteristics to output lower frequency 100MHz for more flexibility. But the IDD characteristics remain the same. So, the values provided in datasheets aren't wrong.

Thanks again for your interest.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.