NUCLEO-N657X0-Q: Confliciting info on number of supported PDM MEMs microphones
Hello,
I have a STM32 NUCLEO-N657X0-Q development board. I wanted to interface with 8 digital PDM MEMs microphones.
In section 68.2 of the STM32N6 reference manual, it states that the N6 supports a "PDM interface, supporting up to 4 microphone pairs". Also in section 2.2.3 of AN5027, it states that if 8 microphone want to be used, the recommended data IO lines are SAI_D1, SAI_D2, SAI_D3, and SAI_D4.
Using CubeMX, I see no option for microphone pair 7-8. In addition to this, SAI_D4 doesn't exist when I search for the pin.
So how do I interface (if possible), the last microphone pair?
Thanks,
Christopher