Skip to main content
Explorer
July 8, 2025
Solved

Parsing UID Fields on STM32L476 – Wafer X/Y Coordinates and BCD Encoding?

  • July 8, 2025
  • 1 reply
  • 297 views

Hi everyone,

I’m working with an STM32L476 and need to parse its 96-bit Unique Device ID (UID).
According to RM0351, the UID starts at address 0x1FFF 7590.

Reading that region with STM32CubeProgrammer gives:

robertkau_1-1752013964577.png

• 0x1FFF 7590 : 0x004A0029
• 0x1FFF 7594 : 0x58335011
• 0x1FFF 7598 : 0x2031374B

So the full UID (high → low) is 0x2031374B 58335011 004A0029.
According to this documentation, the lower 32 bits encode the X/Y coordinates of the die on the wafer, in BCD.

That leaves two questions:

  1. Bit mapping

    • Which 16-bit half-word is X and which is Y?

    • Is it X = bits [31:16] and Y = bits [15:0], or the other way around?

  2. BCD validity

    • If the field is pure BCD (8421), every nibble should be 0-9, yet the value 0x4A contains nibble A (10).

    • Do recent STM32 parts still use BCD for these coordinates, or should those half-words be treated as plain unsigned integers?

Any clarification or official reference would be greatly appreciated.

Thanks!

Best answer by mƎALLEm

Hello,

I've got a confirmation internally regarding question 1: indeed X = bits [15:0]  and Y = bits [31:16].

For the second question you need to an online support request over this link

Thank you

1 reply

mƎALLEm
Technical Moderator
July 11, 2025

Hello,

I can answer the first question,

According to this thread: STM32H7A3 Unique Device ID number question 

X = bits [15:0]  and Y = bits [31:16], I can check.

Meanwhile, I will try to check internally for the format of X/Y and get back to you if I get the information.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
mƎALLEm
mƎALLEmBest answer
Technical Moderator
July 15, 2025

Hello,

I've got a confirmation internally regarding question 1: indeed X = bits [15:0]  and Y = bits [31:16].

For the second question you need to an online support request over this link

Thank you

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."