Skip to main content
CTapp.1
Senior III
March 26, 2026
Solved

Per-device CAN buffer capabilities

  • March 26, 2026
  • 2 replies
  • 175 views

Is there an easy way to find devices that support specific CAN buffer configurations?

For example, some only have receive queues whilst others allow a number of receive buffers to be configured (which is what I want). I know the H7x7 supports this, but does anything else?

Best answer by mƎALLEm

Hello,

To my knowledge there is no way to find that information in a simple way. 

The full configuration of FDCAN is available in STM32H7 family. 

So you need to check the RMs for each STM32 series.

 

2 replies

mƎALLEm
mƎALLEmBest answer
Technical Moderator
March 26, 2026

Hello,

To my knowledge there is no way to find that information in a simple way. 

The full configuration of FDCAN is available in STM32H7 family. 

So you need to check the RMs for each STM32 series.

 

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
CTapp.1
CTapp.1Author
Senior III
March 27, 2026

Also available in the STM32N6(57).

All posts are made in a personal capacityMISRA C++ ChairMISRA C WG MemberDirector The MISRA Consortium Limited (TMCL)
mƎALLEm
Technical Moderator
March 27, 2026

@CTapp.1 wrote:

Also available in the STM32N6(57).


Yes. Generally speaking available in the highest performant MCUs: starting from H7 (currently):

screenshot.png

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."