Skip to main content
Senior
July 8, 2025
Solved

Sleep, stop and standby modes do not significantly reduce current consumption

  • July 8, 2025
  • 5 replies
  • 515 views

Greetings, 
I'm having an issue with low-power modes. I'm using a STM32U585 MCU and while in run mode it is consuming around 100mA, which is a lot. I tried to enter in Sleep, Stop and Standby modes right after the main declaration:

int main(void)
{
 HAL_Init();
 SystemPower_Config();
 SystemClock_Config();
 PeriphCommonClock_Config();

 HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_SLEEPENTRY_WFI);

 ...

The thing is, the current just drops from 100mA to 70mA, which is still a lot. 
Any clue why the circuit is consuming so much current? 

Thank you

 

Best answer by TDK

100 mA is too much for the CPU alone. My guess is other components on the board are using most of that current.

5 replies

j_filipeAuthor
Senior
July 8, 2025

Note: 
In the HAL_PWR_EnterSTOPMode function, the 2nd argument is PWR_STOPENTRY_WFI, not Sleep.

Andrew Neil
Super User
July 8, 2025

You need to give more details: How to write your question to maximize your chances to find a solution.

In particular, what hardware are you using?

How are you measuring the current?

How are you sure you're measuring only the MCU's current consumption?

Have you tried the ST examples on an ST board?

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
KDJEM.1
Technical Moderator
July 8, 2025

Hello @j_filipe;

 

I recommend you to refer to How to minimize the power consumption in low power mode: An example using NUCLEO-F401RE board FAQ to minimize the power consumption. The purpose of this article is to share tips for power consumption optimization while describing steps to achieve it.

Please set all free pins as analog to optimize the power consumption.

I advise you to look at  PWR_STANDBY and PWR_SLEEP examples may help you. 

 

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
TDK
TDKBest answer
Super User
July 8, 2025

100 mA is too much for the CPU alone. My guess is other components on the board are using most of that current.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Andrew Neil
Super User
July 10, 2025

@j_filipe for the benefit of others who may find this while looking to solve a similar problem, it would help if you would say where the excess current was going.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
j_filipeAuthor
Senior
July 10, 2025

Hi Andrew, 
It is irrelevant because I am just using this MCU in a personal project, so it is a personal custom-made board. The excess current was going to another component of the circuit. 
Thank you.

Andrew Neil
Super User
July 11, 2025

Not irrelevant at all: a great example that the MCU is not the only thing which contributes to "low power" - something which is often overlooked!

 

So thanks for sharing.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.