SPI DMA transmit complete interrupt to early
Hello,
I have an STM32G441 and using DMA to transmit some SPI data. All works so far. The problem is the chipselect. I am using the software chipselect. So before I start the DMA I pull CS low. Then when the DMA complete interrupt fires I pull it high again. The problem is, it cuts off about 3 or 4 bytes. This is obvious because the DMA is done while there is still SPI data in the buffer.
What is the go-to solution for this? How can I reliably get an interrupt when the DMA is done and the SPI is done transmitting all data? At the moment I simply start a timer when the DMA is done that triggers a second interrupt after a certain time that I measure with a logic analyzer. Seems a bit makeshift and has to be adjusted each time the baudrate is changed. I also noticed that all the SPI interrupts fire premature. So is it the only solution to waste a timer on the SPI?