Question
Status of USART, SPI and CAN in ST bootloader for STM32L4 ?
New question split from this post.
One additinal request: When checking if bootloader pin configuration has an impact on the real application it would be helpful to know the default level for output pins, like
- does the UART_TX pin drive active high or low?
- does the boot loader drive the SPI MISO output pin HI, LO or Z?
- is the CAN_TX pin drven HI or LOW?
Thank you!