Skip to main content
Associate II
May 15, 2025
Question

STM32 H533 I3C does not ack when sending 7E

  • May 15, 2025
  • 2 replies
  • 649 views

Hello, I'm using two H533 Nucleo Boards and I'm trying to establish an I3C communication between them. There are no specific examples for this protocol using two of these boards, instead there are only examples for a sensor which I don't have. So, I tried to copy the example presented in Introduction to I3C for STM32 MCUs Application Note. This did not work. Also, I tried to adapt the example for the H503 called I3C_Target_ENTDAA_IT, copying the main.c. Also didn't work. The Target is not ack when sending 7E.

On the controller side, I'm just trying to send this:

if (HAL_I3C_Ctrl_DynAddrAssign_IT(&hi3c1, I3C_ONLY_ENTDAA) != HAL_OK){

Error_Handler();

}

On the target side, this is my code:

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file I3C/I3C_Target_ENTDAA_IT/Src/main.c
 * @author MCD Application Team
 * @brief This sample code shows how to use STM32H5xx I3C HAL API to
 * manage a Dynamic Address Assignment procedure between a Controller
 * and Targets with a communication process based on Interrupt transfer.
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2023 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

COM_InitTypeDef BspCOMInit;

I3C_HandleTypeDef hi3c1;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_I3C1_Init(void);
static void MX_ICACHE_Init(void);
static void MX_NVIC_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_I3C1_Init();
 MX_ICACHE_Init();

 /* Initialize interrupts */
 MX_NVIC_Init();
 /* USER CODE BEGIN 2 */
 /* Configure LED2 */
 BSP_LED_Init(LED2);

 /*##- Start the listen mode process ####################################*/
 /* Activate notifications for specially for this example
 - Dynamic address association */
 if( HAL_I3C_ActivateNotification(&hi3c1, NULL, HAL_I3C_IT_DAUPDIE) != HAL_OK)
 {
 /* Error_Handler() function is called when error occurs. */
 Error_Handler();
 }
 /* USER CODE END 2 */

 /* Initialize leds */
 BSP_LED_Init(LED_GREEN);

 /* Initialize USER push-button, will be used to trigger an interrupt each time it's pressed.*/
 BSP_PB_Init(BUTTON_USER, BUTTON_MODE_EXTI);

 /* Initialize COM1 port (115200, 8 bits (7-bit data + 1 stop bit), no parity */
 BspCOMInit.BaudRate = 115200;
 BspCOMInit.WordLength = COM_WORDLENGTH_8B;
 BspCOMInit.StopBits = COM_STOPBITS_1;
 BspCOMInit.Parity = COM_PARITY_NONE;
 BspCOMInit.HwFlowCtl = COM_HWCONTROL_NONE;
 if (BSP_COM_Init(COM1, &BspCOMInit) != BSP_ERROR_NONE)
 {
 Error_Handler();
 }

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);

 while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV1;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLL1_SOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLM = 4;
 RCC_OscInitStruct.PLL.PLLN = 31;
 RCC_OscInitStruct.PLL.PLLP = 2;
 RCC_OscInitStruct.PLL.PLLQ = 2;
 RCC_OscInitStruct.PLL.PLLR = 2;
 RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1_VCIRANGE_3;
 RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1_VCORANGE_WIDE;
 RCC_OscInitStruct.PLL.PLLFRACN = 2048;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
 |RCC_CLOCKTYPE_PCLK3;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure the programming delay
 */
 __HAL_FLASH_SET_PROGRAM_DELAY(FLASH_PROGRAMMING_DELAY_2);
}

/**
 * @brief NVIC Configuration.
 * @retval None
 */
static void MX_NVIC_Init(void)
{
 /* I3C1_ER_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(I3C1_ER_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(I3C1_ER_IRQn);
 /* I3C1_EV_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(I3C1_EV_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(I3C1_EV_IRQn);
 /* EXTI13_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(EXTI13_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(EXTI13_IRQn);
}

/**
 * @brief I3C1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_I3C1_Init(void)
{

 /* USER CODE BEGIN I3C1_Init 0 */

 /* USER CODE END I3C1_Init 0 */

 I3C_FifoConfTypeDef sFifoConfig = {0};
 I3C_TgtConfTypeDef sTgtConfig = {0};

 /* USER CODE BEGIN I3C1_Init 1 */

 /* USER CODE END I3C1_Init 1 */
 hi3c1.Instance = I3C1;
 hi3c1.Mode = HAL_I3C_MODE_TARGET;
 hi3c1.Init.TgtBusCharacteristic.BusAvailableDuration = 0xf8;
 if (HAL_I3C_Init(&hi3c1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure FIFO
 */
 sFifoConfig.RxFifoThreshold = HAL_I3C_RXFIFO_THRESHOLD_1_4;
 sFifoConfig.TxFifoThreshold = HAL_I3C_TXFIFO_THRESHOLD_1_4;
 sFifoConfig.ControlFifo = HAL_I3C_CONTROLFIFO_DISABLE;
 sFifoConfig.StatusFifo = HAL_I3C_STATUSFIFO_DISABLE;

 if (HAL_I3C_SetConfigFifo(&hi3c1, &sFifoConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Target
 */
 sTgtConfig.Identifier = 0xC6;
 sTgtConfig.MIPIIdentifier = 0x1;
 sTgtConfig.CtrlRoleRequest = DISABLE;
 sTgtConfig.HotJoinRequest = DISABLE;
 sTgtConfig.IBIRequest = ENABLE;
 sTgtConfig.IBIPayload = ENABLE;
 sTgtConfig.IBIPayloadSize = HAL_I3C_PAYLOAD_1_BYTE;
 sTgtConfig.MaxReadDataSize = 0xFF;
 sTgtConfig.MaxWriteDataSize = 0xFF;
 sTgtConfig.CtrlCapability = DISABLE;
 sTgtConfig.GroupAddrCapability = DISABLE;
 sTgtConfig.DataTurnAroundDuration = HAL_I3C_TURNAROUND_TIME_TSCO_LESS_12NS;
 sTgtConfig.MaxReadTurnAround = 0x0;
 sTgtConfig.MaxDataSpeed = HAL_I3C_GETMXDS_FORMAT_1;
 sTgtConfig.MaxSpeedLimitation = DISABLE;
 sTgtConfig.HandOffActivityState = HAL_I3C_HANDOFF_ACTIVITY_STATE_0;
 sTgtConfig.HandOffDelay = DISABLE;
 sTgtConfig.PendingReadMDB = DISABLE;
 if (HAL_I3C_Tgt_Config(&hi3c1, &sTgtConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN I3C1_Init 2 */

 /* USER CODE END I3C1_Init 2 */

}

/**
 * @brief ICACHE Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_ICACHE_Init(void)
{

 /* USER CODE BEGIN ICACHE_Init 0 */

 /* USER CODE END ICACHE_Init 0 */

 /* USER CODE BEGIN ICACHE_Init 1 */

 /* USER CODE END ICACHE_Init 1 */

 /** Enable instruction cache in 1-way (direct mapped cache)
 */
 if (HAL_ICACHE_ConfigAssociativityMode(ICACHE_1WAY) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_ICACHE_Enable() != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ICACHE_Init 2 */

 /* USER CODE END ICACHE_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 /* USER CODE BEGIN MX_GPIO_Init_1 */
 /* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();

 /*Configure GPIO pin : PC4 */
 GPIO_InitStruct.Pin = GPIO_PIN_4;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

 /* USER CODE BEGIN MX_GPIO_Init_2 */
 /* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */
/**
 * @brief I3C notify callback after receiving a notification.
 * The main objective of this user function is to check on the notification ID
 * and toggle Led when confirmed or call Error_Handler().
 * @par Called functions
 * - HAL_I3C_NotifyCallback()
 * @retval None
 */
void HAL_I3C_NotifyCallback(I3C_HandleTypeDef *hi3c, uint32_t eventId)
{
 if ((eventId & EVENT_ID_DAU) == EVENT_ID_DAU)
 {
 /* Toggle LED2: Transfer in transmission process is correct */
 BSP_LED_Toggle(LED2);
 }
 else
 {
 /* Error_Handler() function is called when error occurs. */
 Error_Handler();
 }
}

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* Error if LED2 is slowly blinking (1 sec. period) */
 while (1)
 {
 BSP_LED_Toggle(LED2);
 HAL_Delay(1000);
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

With the Analog Discovery 3 Logic Analyzer, i am seeing this:

guillerminaborrazas_0-1747322886498.png

I also tried putting a breakpoint with the debugger at line 357 and it is not reaching it.

 Any ideas what can be happening? Do you have any example between two H533 boards that I could run?
Thank you very much,

Guillermina

2 replies

Associate II
May 16, 2025

When consulting the errata of the H533RE it states the following:

guillerminaborrazas_0-1747417449709.png

 

This was not happening. So I tried calling the function HAL_I3C_Ctrl_DynAddrAssign_IT(&hi3c1, I3C_ONLY_ENTDAA) twice, just in case the Target was set to ignore this first 7E. 

The second time I send this instruction, 7E, the target acknowledges it and the communication flows. 

Any comments or other thing I should bear in mind at the time of working with the I3C peripheral? 

Thank you

Foued_KH
ST Employee
September 12, 2025

Hello @guillerminaborrazas , 

Please ensure your controller is configured correctly. If not, you can refer to the available examples in CubeFW: STM32CubeH5/Projects at main · STMicroelectronics/STM32CubeH5 · GitHub

Foued

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.