Skip to main content
Visitor II
September 12, 2025
Question

STM32 VSCode Build Analyzer: .map file not detected when project folder name differs from target name

  • September 12, 2025
  • 1 reply
  • 998 views

Environment:
- STM32Cube VSCode Extension (with Build Analyzer)
- CMake-based project generated by STM32CubeMX
- Windows 11 / GCC toolchain

Issue:
- The Build Analyzer fails to detect the .map file and reports "NO_MAP_FILE".
- Investigation shows that the analyzer seems to only look for a .map file named after the *project folder*
(e.g. build/Debug/<project_folder>.map).
- However, in CMake projects the actual build target name is derived from ${CMAKE_PROJECT_NAME}, which can differ
from the folder name.
(In my case: project name = VaporChamberController_V2, folder name = VaporChamberController_V2_vscode).

Steps to reproduce:
1. Create a project where the folder name and project name are different.
2. Build the project with CMake.
3. A .map file is generated (using the target name), but the Build Analyzer shows "NO_MAP_FILE".

Workaround:
- Manually force the linker to generate a .map file with the folder name using `target_link_options()`.

Suggestion:
- Modify the Build Analyzer to also check for .map files named after the target (same as the ELF file name).
- Alternatively, provide a VSCode setting that allows the user to configure the .map file name/pattern that the analyzer should use.

This would make the analyzer more robust and prevent confusion when project folder names and target names differ.

1 reply

Explorer
September 16, 2025

I just hit this issue. Pretty annoying. My solution was to make a subfolder with the project name and move everything into that, regenerate with MX, then it was happy.