STM32 with at least 8 DMA channels that can be triggered by and write to GPIOs
Hi.
I'm looking for an STM32 with a lot of GPIO triggered DMA channels. I need 8 channels that trigger when a pin changes state, and which can read/write to GPIO registers and DMA registers.
It's for implementing a bus interface where I need to read address pins and write them into the lower 16 bits of DMA address registers, and use pin transitions to trigger GPIO state changes (GPIO data values, GPIO direction bits).
Are there any parts that can do that? The M0+ series doesn't have enough DMA channels that can be triggered by GPIOs. The M3 and M4 doesn't seem to allow triggering from GPIOs.