Skip to main content
Associate II
August 13, 2025
Question

STM32F1 TIM Input Capture prescaler seems ignored, and OC match doesn’t reset counter — expected behavior?

  • August 13, 2025
  • 1 reply
  • 348 views

Goal

  1. Measure input signal frequency using Input Capture (IC).

  2. Generate a regular waveform using Output Compare (OC) Toggle.


Problem 1 — IC prescaler appears to have no effect

I expected the IC prescaler to capture every Nth edge (e.g., DIV2 → every 2nd event) so that the measured tick delta would scale accordingly. However, regardless of ICPrescaler (DIV1/DIV2/DIV4/DIV8), the capture deltas (and computed frequency) are unchanged.

My configuration (summary):

  • Counter: up-counting, ARR = XXXX, PSC = XXXX

  • IC: rising edge, ICSelection = DIRECTTI, ICFilter = 0, ICPolarity = RISING

  • No slave mode (SMS = 000), no triggers, timer just free-running

  • ICPrescaler = TIM_ICPSC_DIV1 (works), then changed to DIV2/DIV4/DIV8 (register shows the change), but captured values don’t reflect prescaling

  • In debug I can see CCRy values updating and CCxIF asserted correctly

  • Frequency measured (from successive captures with overflow handling) matches the input when DIV1; unchanged when using DIV2/4/8

Questions (IC):

  1. Under what exact conditions does the IC prescaler (CCxPS bits) take effect on STM32F1?

    • Does it require specific edge filters, input mapping (TIx/Indirect/Trig), or slave mode to be active?

  2. Is the IC prescaler supposed to drop/interleave latching into CCR while still asserting CCxIF every edge, or should both be prescaled?

  3. If the prescaler simply skips CCR latching but I compute deltas between successive captured values, should I explicitly divide by the prescale factor in software? (Right now I see no change in the captured deltas.)


Problem 2 — OC match does not reset the counter

When using OC Toggle mode, after a compare match the counter does not reset; the period of the output waveform is governed by ARR, not by the compare value CCR. I can see why (counter only resets at update/ARR), but then:

  • If I want a waveform whose period equals Δ between compare events, do I have to update CCR incrementally in the ISR (e.g., CCR += interval_ticks) so the next event is scheduled relative to the last compare rather than waiting for CNT to roll to ARR?

  • Is there any hardware mode on STM32F1 where a compare match can reset the counter automatically (without using One-Pulse or a slave-mode reset trigger)?

  • Is this behavior (no reset on compare) the general timer design across MCUs, or specific to STM32 F1?

What I tried (OC):

  • OC Toggle with ARR = LARGE, CCR = K → output toggles once per timer period at position K (as expected), overall frequency set by ARR.

  • Resetting CNT in the OC ISR works functionally but slows the output due to ISR latency/jitter (as expected).

  • PWM mode works as a regular waveform generator (ARR = period, CCR = duty), but I was exploring OC behavior specifically.

1 reply

TDK
Super User
August 13, 2025

Counter counts from 0 to ARR. CCRx doesn't affect the period. This is expected. Change ARR to control the period.

You can reset the counter manually, but then it's subject to CPU intervention and jitter.

"If you feel a post has answered your question, please click ""Accept as Solution""."