STM32F4 I2C CR2 Peripheral clock frequency
- April 27, 2026
- 0 replies
- 73 views
Dear Forum,
I'm using a STM32F401 and implemented the I2C as Target transmitter (Slave) answering a I2C question.
I'm programming the I2C CR2 (FREQ Bits) Register as follows with correct speed (42 MHz)
I2C1->CR2 = ((DRV_RCC_GetPCLK1Freq() / 1000000u) & I2C_CR2_FREQ_Msk);I've noticed some spikes when the STM32 I2C controller generates the answer, see below (yellow markings)

Blue: Clock generated by the controller (the clock speed is about 200kHz)
Red: Adrdess Byte generated by the controller, Data Bytes generate by STM32 I2C transmitter (answer) with spikes
When the FREQ Bits of I2C_CR2 Register are zero, this spikes doesn't occur, see below

The Reference Manual RM0368 Rev 6 for the I2C CR2 writes:

It is noticed that this FREQ bits must be configured to generate I2C compliant Signals. Anyhow from EMC perspective this spikes are bad because the radiate a wide spectrum. I've found nowhere information of correct I2C specifiation/behaviour of the Data Signal the be compliant, anyhow the data is transfered correctly to the controller.
Q: must the FREQ bit of CR2 be set in slave mode?
Q: what is I2C compliant behaviour
Q: How about CCR Register, is it neccessary to set in slave mode (how to set the I2C_CCR_FS Flag)?
Q: Is this Standard or Fast Mode (because of 200 kHz clock)?
Q: TRISE Register doen't show any influence if this case, is it of any concern?
Thank you for your thoughts and time.
regards,
Lorenz