Skip to main content
Visitor II
September 15, 2025
Question

STM32F4 low-power mode not waking up with external interrupt

  • September 15, 2025
  • 1 reply
  • 376 views

Hi all,

I’m working on a project using an STM32F407 and running into issues with low-power modes. I can put the MCU into STOP mode successfully, but when I try to wake it up with an external interrupt (EXTI line on a GPIO pin), nothing happens. The device just stays stuck until I reset it manually.

Here’s what I’ve tried so far:

  • Configured the EXTI line with rising-edge trigger.

  • Verified the interrupt works fine when the MCU is running normally.

  • Enabled the corresponding NVIC interrupt before entering STOP mode.

  • Added __WFI() after setting STOP mode in the power control register.

Despite this, the MCU never wakes up when the pin is toggled. I must be missing something in the clock or power configuration, but I can’t figure it out.

Has anyone dealt with this before on STM32F4 (or similar STM32 family)? Any pointers on debugging wake-up sources in STOP mode would be a huge help.

Thanks!

1 reply

TDK
Super User
September 15, 2025
"If you feel a post has answered your question, please click ""Accept as Solution""."