Skip to main content
Visitor II
September 7, 2025
Question

STM32F405RGT6 package

  • September 7, 2025
  • 2 replies
  • 273 views

I have received some STM32F405RGT6 microcontrollers that have two circular marks (holes) on the package, while the official datasheet only shows one mark indicating pin 1.

Is there an official revision or packaging variant from STMicroelectronics that includes two marks?

Additionally, does having two marks indicate that the part might be counterfeit or not authentic?

Could you please provide official documentation or images to clarify this

2 replies

STTwo-32
Technical Moderator
September 7, 2025

Hello @LisaLisi and welcome to the ST Community.

according to the DS8626, the MCU you are asking about is a LQFP64 (10 x 10mm). So, referring to the TN1433, the marking on the package top view is exactly as follow:

STTwo32_0-1757239589443.png

So, check if your MCU follow this model. If it is not, please send me a privet message on the ST Community that include a picture of your MCU.

Best Regards.

STTwo-32

 

AScha.3
Super User
September 7, 2025

If you just see two "marks" , dont worry about, only one is pin1 marking; more might come from the package.

see image from rs :

AScha3_0-1757241713279.png

This is as it should look.

"If you feel a post has answered your question, please click ""Accept as Solution""."