Skip to main content
Associate II
June 12, 2025
Solved

STM32F767 ROM Bootloader over I2C: Should Mass Erase work?

  • June 12, 2025
  • 4 replies
  • 443 views

Hello World;

My Setup:

  • Nucleo F767ZI Board
  • BOOT0 pulled high
  • SCL/SDA on PB6/PB9 connected to Raspberry Pi I2C-1 and Saleae Logic Pro 8
  • Nucleo board powered via USB from Raspberry Pi

Goal: Using ROM Bootloader over I2C for firmware updates (later on custom hardware)

Problem: I2C hangs after issuing Mass Erase command

STM32F767-MassErase.png

 

 

 

 

 

Send: 0x45 0xBA Erase-NS Command

Receive: 0x79 ACK

Send 0xff 0xff 0x00 Special Erase

Receive for ACK or NAK hangs while sending the I2C device address.

AN4221 says "Some products do not support the mass erase feature." Does STM32F767 support mass erase?

 

 

Best answer by TDK

Read the flash size register.

TDK_0-1749822930242.png

 

4 replies

TDK
Super User
June 12, 2025

Looks like you eventually get an ACK based on your logic analyzer screenshot. How long does this take? Is the flash erased after this?

Does the regular Mass Erase command work (0x44 0xBB)?

Setting RDP 1 then reverting to RDP 0 will also mass erase the flash.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate II
June 13, 2025

@TDK wrote:

Does the regular Mass Erase command work (0x44 0xBB)?

I don't know. Currently I'm using the stm32flash 0.7 tool from here https://sourceforge.net/projects/stm32flash/ , and this happens to use this specific command. My plan was to avoid writing my own tool, but I may have to do so.

Tesla DeLorean
Guru
June 12, 2025

I'd expect it to work, but could take it's time to complete, and might cause the processor to stall and not be responsive to real-time interaction. 

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
Associate II
June 13, 2025

Ok, I started to make my own tool, and it seems to work now. Takes about 16s for a 2MB part.

STM32F767 is available with 1MB or 2Mb of flash? How do I know which type I have? The ID is the same for all of them.

 

TDK
Super User
June 13, 2025

What chip do you have? There are more letters after STM32F67 that indicate flash size.

TDK_0-1749822705364.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate II
June 13, 2025

I'd rather like the bootloader client to figure this out automatically.

 

TDK
TDKBest answer
Super User
June 13, 2025

Read the flash size register.

TDK_0-1749822930242.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."