stm32g030 RTC/LSI ticks 50% too often
Hi!
I use the RTC of a STM32G030K6T. It is clocked by LSI (appr. 32kHz). And PREDIV_A is 0x0 and PREDIV_S is 0x7FFF. So I expect that RTC_SSR overflows every 1.024sec...
But: It overflows every 0.687sec... As if the LSI frequency would be 47712Hz...
I mentioned this after I soldered the positive contact of a LiFePO4 battery... Now I cannot easily disconnect power... Triggering the reset pin does not change the fast RTC... A software reset does not help, too...
How could I possibly damage the LSI by making a solder joint at the other side of the board? I even have a voltage clamp at 3.5V and a LDO (3.0V) between that solder joint and the STM32G030.
Or is it more likely that I made some last minute firmware changes? What could that be?
Thx.
Bye.