Skip to main content
Associate II
February 18, 2026
Question

STM32G0B0: Errors in RM0454 regarding Flash ?

  • February 18, 2026
  • 1 reply
  • 185 views

Split from STM32G0B0: RM0454 link out-of-date ? - this is a new topic raising issues in the document itself.


Hi @Amel NASRI ,

Thank you for your quick answer.

I have however encountered a few errors in that RM0454 Rev 5 that are different/fixed in RM0444 Rev 6. For example, the following is all done on an STM32G0B0CE (512kiB) rev Z.

  • Erasing a flash page (page 78/989) PNB's limit should be 128 so it stays limited to the 256KiB of the selected bank using BKER. A higher value (for example 256+) errors the flash controller.
    If this is correct, the following image should also be incorrect (Table 9, pg 55/989)

    massimogPVS_0-1771424304318.png
    and be changed to
    massimogPVS_1-1771424817397.png
  • Another issue that I encountered is that the 512kiB STM32G0B0CE sometimes bricks when attempting to change the option byte DUAL_BANK (pg 81/989)
    massimogPVS_2-1771424886850.png

    I believe this should also be as in RM0444, 512kiB devices always operate in DUAL_BANK mode.

    massimogPVS_3-1771425224826.png

     

Have I looked over something that caused me these issues? Or could you confirm that these are indeed errors in RM0454?

Hope to hear from you soon!

1 reply

Amel NASRI
Technical Moderator
February 20, 2026

Hi @massimogPVS ,

 

Please let me check and confirm whether your assumption about missing updates in RM0454 compared to RM0444 is correct.

I have submitted an internal ticket on this topic: 227689 (this is an internal tracking number and is not accessible or usable by customers).

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.