Skip to main content
LPetr.1
Senior
July 8, 2025
Solved

STM32G0B1V issue with ADC measurements

  • July 8, 2025
  • 3 replies
  • 439 views

I am having issues with the STM32G0 ADC measurements. I am trying to measure 2 voltages:

1. 3.3V

LPetr1_0-1751962592906.png

2. 12V

LPetr1_1-1751962700508.png


After the voltage divider, the 3.3_adc and 12v adc pins are connected to the MCU pins directly:

3.3_adc - PA3 (ADC1_IN3)

12v adc - PA7 (ADC1_IN7)

My STM32CubeMX configuration for the ADC is as following:

LPetr1_2-1751962920393.png



VREFBUF Mode is configured as External voltage reference:

LPetr1_3-1751962943488.png



Because we have 2.5V connected to the VREF+ pin of the MCU and we want to use it as the ADC Reference Voltage, see the schematic below:

LPetr1_4-1751963007277.png



I have measured the voltages with the Multimeter on VREF+, +3.3V and +12V, and all of them are correct and as expected. I have also measured the voltages using multimeter after the Voltage divider and I measure as following:

3.3_adc - 0.275V (if I apply voltage divider, I get 3.3V precisely)

12v adc - 0.508 (if I apply voltage divider, I get about 11.6V. This is expected voltage on this pin as it has some diode connected on this line hence its not actually +12V)


My code is as following:

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2025 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "stdio.h"
#include "printf.h"

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc1;
DMA_HandleTypeDef hdma_adc1;

UART_HandleTypeDef huart3;

/* USER CODE BEGIN PV */
uint32_t AD_RES_BUFFER[2];

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_USART3_UART_Init(void);
static void MX_ADC1_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

static float ConvertToVoltage(uint32_t adc_value,float multiplier)
{
 return ((float)adc_value / 4095.0f) * 2.5f*multiplier;
}

void HAL_ADC_ConvHalfCpltCallback(ADC_HandleTypeDef* hadc)
{
 // Maybe process first half of buffer
}

void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)
{
 // Maybe process full buffer
}

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */
 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_USART3_UART_Init();
 MX_ADC1_Init();
 /* USER CODE BEGIN 2 */
 HAL_ADC_Start_DMA(&hadc1, AD_RES_BUFFER, 2);

 printf("hello \n");

 uint32_t vref_csr = VREFBUF->CSR;

 uint8_t envr = (vref_csr & VREFBUF_CSR_ENVR) ? 1 : 0;
 uint8_t hiz = (vref_csr & VREFBUF_CSR_HIZ) ? 1 : 0;
 uint8_t vrs = (vref_csr & VREFBUF_CSR_VRS) ? 1 : 0;

 printf("vref_csr envr = %u \n", envr);
 printf("vref_csr hiz = %u \n", hiz);
 printf("vref_csr vrs = %u \n", vrs);







 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {

 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */

	 printf("ADC IN3 = %u \n",AD_RES_BUFFER[0]);
	 printf("ADC IN7 = %u \n",AD_RES_BUFFER[1]);
	 printf("ADC IN3 raw voltage = %.2f\n",(AD_RES_BUFFER[0] / 4095.0f) * 2.5f);
	 printf("ADC IN7 raw voltage = %.2f\n",(AD_RES_BUFFER[1] / 4095.0f) * 2.5f);
	 printf("ADC IN3 voltage = %.2f \n",ConvertToVoltage(AD_RES_BUFFER[0],12.0f));
	 printf("ADC IN7 voltage = %.2f \n",ConvertToVoltage(AD_RES_BUFFER[1],23.0f));
	 printf("\n");
 HAL_Delay(1000);


 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV1;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV1;
 RCC_OscInitStruct.PLL.PLLN = 8;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
 RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
 RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief ADC1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_ADC1_Init(void)
{

 /* USER CODE BEGIN ADC1_Init 0 */

 /* USER CODE END ADC1_Init 0 */

 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC1_Init 1 */

 /* USER CODE END ADC1_Init 1 */

 /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV2;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc1.Init.LowPowerAutoWait = DISABLE;
 hadc1.Init.LowPowerAutoPowerOff = DISABLE;
 hadc1.Init.ContinuousConvMode = ENABLE;
 hadc1.Init.NbrOfConversion = 2;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc1.Init.DMAContinuousRequests = ENABLE;
 hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc1.Init.SamplingTimeCommon1 = ADC_SAMPLETIME_160CYCLES_5;
 hadc1.Init.SamplingTimeCommon2 = ADC_SAMPLETIME_160CYCLES_5;
 hadc1.Init.OversamplingMode = DISABLE;
 hadc1.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_HIGH;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_3;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLINGTIME_COMMON_1;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_7;
 sConfig.Rank = ADC_REGULAR_RANK_2;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */

 /* USER CODE END ADC1_Init 2 */

}

/**
 * @brief USART3 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_USART3_UART_Init(void)
{

 /* USER CODE BEGIN USART3_Init 0 */

 /* USER CODE END USART3_Init 0 */

 /* USER CODE BEGIN USART3_Init 1 */

 /* USER CODE END USART3_Init 1 */
 huart3.Instance = USART3;
 huart3.Init.BaudRate = 115200;
 huart3.Init.WordLength = UART_WORDLENGTH_8B;
 huart3.Init.StopBits = UART_STOPBITS_1;
 huart3.Init.Parity = UART_PARITY_NONE;
 huart3.Init.Mode = UART_MODE_TX_RX;
 huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart3.Init.OverSampling = UART_OVERSAMPLING_16;
 huart3.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 huart3.Init.ClockPrescaler = UART_PRESCALER_DIV1;
 huart3.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 if (HAL_UART_Init(&huart3) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetTxFifoThreshold(&huart3, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetRxFifoThreshold(&huart3, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_DisableFifoMode(&huart3) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USART3_Init 2 */

 /* USER CODE END USART3_Init 2 */

}

/**
 * Enable DMA controller clock
 */
static void MX_DMA_Init(void)
{

 /* DMA controller clock enable */
 __HAL_RCC_DMA1_CLK_ENABLE();

 /* DMA interrupt init */
 /* DMA1_Channel1_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn);

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOF_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */


The result:

hello 
vref_csr envr = 0 
vref_csr hiz = 1 
vref_csr vrs = 0 
ADC IN3 = 585 
ADC IN7 = 968 
ADC IN3 raw voltage = 0.36
ADC IN7 raw voltage = 0.59
ADC IN3 voltage = 4.32 
ADC IN7 voltage = 13.59 

ADC IN3 = 585 
ADC IN7 = 969 
ADC IN3 raw voltage = 0.36
ADC IN7 raw voltage = 0.59
ADC IN3 voltage = 4.29 
ADC IN7 voltage = 13.58 

ADC IN3 = 587 
ADC IN7 = 970 
ADC IN3 raw voltage = 0.36
ADC IN7 raw voltage = 0.59
ADC IN3 voltage = 4.29 
ADC IN7 voltage = 13.59 


I cannot wrap my head around what could be the issue.

I have double checked the actual voltages on the 3.3V and 12V before and after voltage divider and they are CORRECT.

I have double checked the actual voltage on the VREF+ pin and it is precisely 2.5V

 

So there should not be any Hardware related faults, so it must be the configuration issue in the code but I cannot figure out what it could be. I would appreciate if someone could help me with this issue and point me in the right direction what else I can do to debug this.

 

Best answer by Karl Yamashita

You need to calibrate the ADC first. Call HAL_ADCEx_Calibration_Start before starting the DMA

 

/* USER CODE BEGIN 2 */
 HAL_ADCEx_Calibration_Start(&hadc1);
 HAL_ADC_Start_DMA(&hadc1, AD_RES_BUFFER, 2);

 printf("hello \n");

 

3 replies

waclawek.jan
Super User
July 8, 2025

Your input signal is of high impedance, so  make sure the sampling time is set adequately.

JW

TDK
Super User
July 8, 2025

You must calibrate the ADC after startup and before use.

TDK_0-1751985384723.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
LPetr.1
LPetr.1Author
Senior
July 9, 2025

That was totally the issue. I completely missed that from the reference manual. Though I am very surprised that the offset was so large before calling the calibration (almost 1V)

Karl Yamashita
Karl YamashitaBest answer
Principal
July 8, 2025

You need to calibrate the ADC first. Call HAL_ADCEx_Calibration_Start before starting the DMA

 

/* USER CODE BEGIN 2 */
 HAL_ADCEx_Calibration_Start(&hadc1);
 HAL_ADC_Start_DMA(&hadc1, AD_RES_BUFFER, 2);

 printf("hello \n");

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source