STM32G4: Wrong description of HRTIM_ADCxR registers in RM0440 Rev 9
If I am correct, the descriptions of
- HRTIM_ADC2R
- Bit 22
- HRTIM_ADC3R
- Bit 19
- Bit 13
- HRTIM_ADC3R
- Bit 22
- Bit 13
- Bit 10
- Bit 5
- Bit 4
- Bit 0
are not correct in the RM.
They all describe trigger event generation but the trigger output in all these seem wrong:
E.g.: HRTIM_ADC2R, Bit 22,
Original Text: "This bit enables the generation of an ADC trigger upon timer C reset and roll-over event, on ADC trigger 1 output."
It should be: "This bit enables the generation of an ADC trigger upon timer C reset and roll-over event, on ADC trigger 2 output."
Also, I want to ask, if this forum is the right place to give feedback on documentation issues?
Best Simon