STM32G474 HRTIMER Deadtime on skipped pulse.
I've STM32G474 using the HRTIMER to control a boost converter, each channel has it's own converter. This all works nicely with the deadtime, no issues. When I come to do a pulse skip, (set CMP3 to 0) the deadtime is still being inserted in the the Tx2 output even though Tx1 output is not being pulsed! Is this normal or have I missed something?
I've tried a few things to not make the deadtime happen, like disabling the set and reset sources... the only thing that fixes the problem is to also set the falling deadtime to 0 and then subsequently resetting it back to the required value. Tx2 has no set or reset sources configured.