STM32H5E4/E5/F4/F5 with PLAY: boards availability?
A new STM32 sub-family (as part of the 'H5 family) came out. They have everything but the kitchen sink. As far as I can tell, 'H5E4 and 'H5E5 differ only in that the higher one has USB-HS with PHY (the 'H5Fx are crypto-enabled variants, as usually)
What's new is also the PLAY peripheral, which is a small programmable logic element, fully documented and configurable through registers. It's based around 16 simple logic elements (4-input LUT and an optional register), complete with an extensive input multiplexer matrix+filter, interconnected to a variety of peripherals (timers, DMA, ADC...) and also GPIO.
I wonder, if there's a Disco around...
JW