STM32H7 USB VBUS sensing question
I am using the USB OTG FS on the STM32H7. My MCU is self powered, so I need to use VBUS sensing. Can a 3.3V signal be used for the VBUS sensing on PA9 or must it be 5V? Based on the linked forum, I believe 3.3V would work, but would like to confirm with the STM32H7 series.
https://community.st.com/t5/stm32-mcus/management-of-vbus-sensing-for-usb-device-design/ta-p/49485#:~:text=On%20STM32F2/F4/F7/,136):
How should I configure OTG_FS_ID PA10 so my MCU is device only? Should I leave it floating, pulled to LOW, or pulled HIGH?
Thanks in advance for any help on this topic.