Skip to main content
Associate III
July 17, 2025
Solved

STM32H743XGH6 PLL1 DIVP1: Is divide by 1 possible?

  • July 17, 2025
  • 2 replies
  • 292 views

Is it possible to divide by 1 for DIVP of PLL1?

According to RM0433 Rev8, DIVP of PLL1 is capable of dividing by 1.
However, I could not set division by 1 in CubeIDE. (It is possible that my setting is incorrect.)

2 replies

Andrew Neil
Andrew NeilBest answer
Super User
July 17, 2025
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
NiMAuthor
Associate III
July 18, 2025

Thank you very much.
It was very helpful.

It was the very answer I wanted to know.

mƎALLEm
Technical Moderator
July 17, 2025
"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."